A method to dynamically estimate the diffusion boundary layer from local velocity conditions in laminar flows

Printer-friendly versionPDF version
International Journal of Heat and Mass Transfer
Pages: 
1563–1571
Volume: 
48
Issue: 
8
Date: 
Tuesday, January 4, 2005
DOI: 
http://dx.doi.org/10.1016/j.ijheatmasstransfer.2004.10.024

The differential equation for dilute species transport next to a planar interface within the hydrodynamic boundary layer is transformed into a differential equation for the diffusion boundary layer. This differential equation contains two coefficients, which depend explicitly on the concentration profile. We show that these coefficients can be taken as identical constants, in a number of limiting cases. Using these constants, we show that this equation reproduces very well the temporal and spatial profile of the diffusion boundary layer determined from numerical simulations in some more complex intermediate cases. The final differential equation depends only on the diffusion coefficient and on local velocity and velocity gradients next to the interface, and not explicitly on concentration. Therefore this equation can be used to estimate the mass transfer coefficient from the local velocity profile when conditions are not fixed in space or time, and especially in transient computational fluid dynamics calculations. It can also be used to estimate new correlations for the mass transfer coefficient, in cases where the spatial velocity profile at the interface is known.

Rights: 
2004 Elsevier Ltd. All rights reserved.
Author Name: 
Fabien Jousse
Thibauld Jongen
Wim Agterof