Modeling Solids Conveying Using the Discrete Element Method
Date: 
Thursday, December 11, 2014
Description: 

Conveying and transport of solids poses challenging problems when compared to the transport of fluids. Particles have a unique flow and transport behavior that is dependent on the shape and size of particles, as well as the geometry and means of transport. Traditional methods of designing particle transport systems rely on experience, correlations and basic principles of physics. Experimentation is necessary to verify the designs.

Simulation, specifically using the Discrete Element Method (DEM), can be employed to assess the suitability of designs. It is a technique where the flow and transport of solids is numerically calculated using the basic laws of motion. Nuances due to shape, size, friction and geometrical parameters can be studied in a scientific manner to evaluate and optimize transport system designs.

This webcast introduces the DEM available within STAR-CCM+® and its application to particle transport. A live demonstration shows how a system simulation and various property parameters of material can both be set up. Examples are presented showing the application of this method to particle transport.

Industries: 
Speaker: 
Ravindra Aglave
Oleh Baran
Speaker Company: 
CD-adapco
Products: