Technical Library

Some articles have copyright restrictions,
in order to download these you will be redirected to the copyright holder's website.

 
Name Author(s) Datesort ascending
Developpement and Validation of extented two-phase computational fluid dynamics model for analysis of boiling flow in reactor fule assemblies Adrian Tentner, W. David Pointer, Tanju Sofu, David Weber, Simon Lo, Andrew Splawski May 13, 2007
Numerical studies on rib&channel dimension of flow-field on PEMFC performance S. Shimpalee, J.W. Van Zee May 1, 2007
Prediction of transient response for a 25-cm2 PEM fuel cell S. Shimpalee, D. Spuckler, J.W. Van Zee February 13, 2007
A coupled CFD-population balance approach for nanoparticle synthesis in turbulent reacting flows Ethro Akroyd, Alastair J. Smith, Raphael Shirley, Laurence R. McGlashan, Markus Kraft February 9, 2007
Numerical Investigations on Methods to Control the Rate of Heat Release of HCCI Combustion Using Reduced Mechanism of N-Heptane With a Multidimensional CFD Code F. Maroteaux, L. Noel, A. Ahmed January 1, 2007
Numerical Modelling of Ship Stern Flows P. L. Nielsen January 1, 2007
Investigation of gas diffusion media inside PEMFC using CFD modeling S. Shimpalee, U. Beuscher, J.W. Van Zee December 7, 2006
Development of Optimization Techniques for the Design of an Internal Combustion Engine Airbox Ciaran Branney, Geoffrey Cunningham, Stephen Spence, Geoffrey McCullough November 13, 2006
CFD Simulations of Heat Transfer from Air Cooled Engines A. Baird, D. Thornhill, G. Cunningham, P. Troxler, B. Price November 13, 2006
The impact of channel path length on PEMFC flow-field design S. Shimpalee, S. Greenway, J.W. Van Zee September 29, 2006
Large Eddy Simulation of Turbulent Channel Flow with Heat Transfer at Low Reynolds and Mach Numbers M. Popov, K. Mikhaylyukov, A. Ryabov, F. Mendonça, C. Tzanos September 25, 2006
Advances in Computational Fluid Dynamics Modeling of Two Phase Flow in a Boiling Water Reactor Fuel Assembly Adrian Tentner, Simon Lo,Andrey Ioilev, Vladimir Melnikov, Maskhud Samigulin, Vasily Ustinenko, Valentin Kozlov July 17, 2006
Evaluation of bespoke and commercial CFD methods for a UCAV configuration M.E. Milne, M.T. Arthur June 5, 2006
Conjugate Heat Transfer Analysis of a Cooled Turbine Vane Using the V2F Turbulence Model Jiang Luo, Eli H. Razinsky June 5, 2006
Inverse modeling and numerical optimization of heater temperatures in a bridgman process J. Jakumeit, M. Emmerich, F. Hediger May 28, 2006
Fully coupled multi-phase mold-filling and solidification simulation of industrial casting processes J. Jakumeit, T. Barth, M. Grauer, J. Reichwald May 28, 2006
Grid computing for casting simulations J. Jakumeit, T. Barth, M. Grauer, J. Reichwald May 28, 2006
High heat-flux accelerator targets: Cooling with liquid metal jet impingement I. Silvermana, A.L. Yarin, S.N. Reznik, A. Arenshtam, D. Kijet, A. Nagler April 18, 2006
Turbulent Natural Convection in Horizontal Coaxial Cylindrical Enclosures: LES and RANS Models Y. Addad, D. Laurence, M. Rabbitt January 1, 2006
Application of computational fluid dynamics to spray drying Simon LO July 5, 2005
Sensitivity study for the mass transfer at a single droplet A.R. Paschedag, W.H. Piarah, M. Kraume July 1, 2005
Features of convective heat transfer in heated helium channel flow S. Gordeev, V. Heinzel, V. Slobodtchouk July 1, 2005
Simulation of Sloshing Loads on Moving Tanks M. Perić, T.Zorn June 12, 2005
Optimal Sunroof Buffeting Predictions with Compressibility and Surface Impedance Effects Alex Read, Fred Mendonca, Christophe Schram, Michel Tournour, Kenneth Karbon May 23, 2005
LES in a U-Bend Pipe Meshed by Polyhedral Cells C. Moulinec, S. Benhamadouche, D. Laurence, M. Perić May 23, 2005
Hybrid atomistic–continuum method for the simulation of dense fluid flows Thomas Werder, Jens H. Walther, Petros Koumoutsakos May 1, 2005
A single-phase, non-isothermal model for PEM fuel cells Hyunchul Ju, Hua Meng, Chao-Yang Wang May 1, 2005
A method to dynamically estimate the diffusion boundary layer from local velocity conditions in laminar flows Fabien Jousse, Thibauld Jongen, Wim Agterof January 4, 2005
Large Eddy Simulations of the Flow Around High-Speed Trains Cruising Inside Tunnels Ben Diedrichs, Mats Berg, Siniša Krajnovi July 24, 2004
Predicting water and current distributions in a commercial-size PEMFC S. Shimpalee, S. Greenway, D. Spuckler, J.W. Van Zee a June 8, 2004
Influence of Turbulence Modeling on Airfoil Unsteady Simulations of Broadband Noise Sources Stephane Moreau, Fred Mendonca, Omar Qazi, Robert Prosser, Dominique Laurence May 23, 2004
DES Validations of Cavity Acoustics over the Subsonic to Supersonic Range Richard Allen, Fred Mendonca May 10, 2004
ADVANCES IN CFD ANALYSIS FOR TRANSIENT TURBOCHARGER FLOWS Fred Mendonça, Stephen Ferguson, Dean Palfreyman November 1, 2003
Large eddy simulation of a forward–backward facing step for acoustic source identification Y. Addad, D. Laurence, C. Talotte, M.C. Jacob August 1, 2003
CFD PREDICTION OF NARROWBAND AND BROADBAND CAVITY ACOUSTICS AT M=0.85 Fred Mendonça, Richard Allen, Julien de Charentenay, David Kirkham May 12, 2003
Modelling of Two–Phase Direct Cylinder Injection Philip R. De Vos January 1, 2003
A Comparison of Modeled and Measured 3-D In-Cylinder Charge Motion Throughout the Displacement of a Four-Valve SI Engine Hans G. Hascher, Harold J. Schock, Oshin Avanessian, James Novak January 1, 2003
Success of STAR-CCM+ Application in the Design Process of Modern Gas Turbine Moritz Norbert様
STAR-CCM+® Usage for Sorbent Injection Optimization Tyler Derritt
Analysis of the Lubrication System in a High Pressure Piston Water Pump Davide Bottazzi, D. Galloni, M. Milani, L. Montorsi
Increasing Exchanger Capacity with CFD Mike Porter, President and Principal Engineer
STAR-CCM+ Modeling of Steel Making Processes Simon Lo
STAR-CCM+による小型垂直軸風車の特性解析 原 豊先生
汽车天窗风振性能研究
STAR-CCM+ Simulations of In-Situ Thermal Treatment of Oil-Shale Michal Hradisky
Fluid-Structure Interaction using STAR-CCM+ and Abaqus Co-Simulation Alan Mueller
Numerical study of cavitating flow inside a flush valve Annie-Claude BAYEUL-LAINẺ, Sophie SIMONET, Guy CAIGNAERT
Prediction of Resistance of Floating Vessels D. Jürgens, M. Palm, M. Perić, E. Schreck
Battery Modeling Solutions Gaetan Damblanc
遠心型血液ポンプ設計におけるOptimate+を用いた最適化設計の検討 森 武寿様

Pages