Technical Library

Some articles have copyright restrictions,
in order to download these you will be redirected to the copyright holder's website.

 
Name Author(s) Datesort ascending
Distribution and Magnitude of Shear Stress after Coronary Bifurcation Lesions Stenting with the Classical Crush Technique: A New Predictor for In-Stent Restenosis Z.H. Hu, S.L. Chen, J.J. Zhang, S.J. Shan, Z.Z. Liu, F. Ye, J. Kan, H.M. Xu, K. Nguyen, T. Kwan, T. Nguyen, T. Hoang August 1, 2010
Contradictory Shear Stress Distribution Prevents Restenosis after Provisional Stenting for Bifurcation Lesions J.J. Zhang, S.L. Chen, Z.Y. Hu, J. Kan, H.M. Xu, S.J. Shan, Z.Z. Liu, F. Ye, T.W. Kwan, K. Nguyen, A. Nanjundappa, T. Nguyen August 1, 2010
Modeling of LOX/Methane Impingement, Mixing and Combustion Naimish B, Harpal, Eric Besnard, Reza Toossi July 25, 2010
Prediction of a subcooled boiling flow with the mechanistic wall boiling and bubble size models B.J. Yun, A. Splawski, S. Lo, C.–H. Song July 23, 2010
Development of CFD Simulation for 3-D Flooding Flows and Scouring Around Bridge Structures B.R.TULIMILLI, P.MAJUMDAR, M.KOSTIC, S.A.LOTTES July 22, 2010
COMPUTATIONAL THERMAL ANALYSIS OF MULTIPLE DISC TYPE ROTARY MAGNETIC REFRIGERATION SYSTEM SHANMUGAM PEREZHIL VENDAN, VEERAPADMANABAN VEERAKRISHNAN, ESAKKIAPPA GOMATHINAYAGAM VINAYAGASUNDARAM July 1, 2010
Pickup Trucks - Box Configuration and Drag Reduction W. A. Mokhtar, R. Camp June 28, 2010
Near-Field Characteristics of Wall Jets with Tabs C. A. Orrala, J. Ji, H. Hoang, H.R. Rahai June 28, 2010
CFD Simulation of Biomass Pyrolysis Syngas vs. Natural Gas in a Microturbine Annular Combustor F. Fantozzi, P. Laranci, G. Bidini June 14, 2010
Benchmarking CD-Adapco's Star-CCM+ in a Production Design Environment Mikhail M. Grigoriev, Chester V. Swiatek,, James A. Hitt June 14, 2010
Heat Transfer Investigations in Multiple Impinging Jets at Low Reynolds Number A. G. Rao, M. Kitron-Belinkov, V. Krapp, Y. Levy June 14, 2010
Experimental Investigation of Laminar Flame Speeds for Medium Calorific Gas With Various Amounts of Hydrogen and Carbon Monoxide Content at Gas Turbine Temperatures Ivan R. Sigfrid, Ronald Whiddon, Robert Collin, Jens Klingmann June 14, 2010
Development in Gas Turbine Repairs A. Thomson, D. A. Anderton June 14, 2010
Experimental and Numerical Analysis of Transport in Saturated Heterogeneous Media S. J. Harrington June 3, 2010
A Computational Fluid Dynamics Study of Air Mixing in a Naturally Ventilated Livestock Building with Different Porous Eave Opening Conditions T. Norton, J. Grant, R. Fallon, D.W. Sun June 1, 2010
Investigation of Unfavorable Winds Associated with Complex Terrain using Detached Eddy Simulation C.H. Hu May 23, 2010
Drag reduction through special paints coated on the hull P. IZAGUIRRE-ALZA, L. PÉREZ-ROJAS, J.F. NÚÑEZ-BASÁÑEZ May 20, 2010
Effect of Design Modifications of Intra-Bore Region on Engine Block Bore Distortion D. Manav, S. Erpolat, K. Ozdemir May 5, 2010
Vehicle Driving Cycle Performance of the Spark-less DI-JI Hydrogen Engine A. A. Boretti May 1, 2010
Effect of Intake Channel Design to Cylinder Charge and Initial Swirl Eero Antila, Ossi Kaario, Matteo Imperato , Martti Larmi April 13, 2010
A Numerical Analysis on Air-cooling Performance of Passenger Cars April 12, 2010
Continued Study of the Error and Consistency of Fan CFD MRF Models P. Gullberg, L. Löfdahl, P. Nilsson, S. Adelman April 12, 2010
Thermal Stress and Thermo-Electrochemical Analysis of a Planar Anode-Supported Solid Oxide Fuel Cell: Effects of Anode Porosity L.K. Chiang, H.C. Liu, Y.H. Shiu, C.H. Lee, R.Y. Lee April 2, 2010
Modelling Auto Ignition of Hydrogen in a Jet Ignition Pre-chamber A. A. Boretti April 1, 2010
Optimising the Ventilation Configuration of Naturally Ventilated Livestock Buildings for Improved Indoor Environmental Homogeneity T. Norton, J. Grant, R. Fallon, D.W. Sun April 1, 2010
Numerical investigation of DQMoM-IEM as a turbulent reaction closure Jethro Akroyd, Alastair J. Smith, Laurence R. McGlashan, Markus Kraft March 15, 2010
Cavitation Enhancement of Silt Erosion: Numerical Studies P. J. Dunstan, S. C. Li March 9, 2010
Numerical Simulation of Friction Stir Butt Welding Process for AA5083-H18 Sheets D. Kim, H. Badarinarayan, J. H. Kim,, C. Kim, K. Okamoto, R.H. Wagoner, K. Chung March 1, 2010
Mesh Optimization for Ground Vehicle Aerodynamics Nor Elyana Ahmad, Essam Abo-Serie, Adrian Gaylard March 1, 2010
Applications of Large Eddy Simulations in Nuclear Field J.P. Simoneau, J. Champigny, O. Gelineau February 1, 2010
Mechanical Erosion of Graphite Nozzle Material in Solid-Propellant Rocket Motors P. Thakre, R. Rawat, R. Clayton January 4, 2010
Advances in the development and validation of CFD-BWR , a Two-Phase Computational Fluid Dynamics model for the simulation of flow and heat transfer in Boiling Water Reactors Adrian Tentner, Simon Lo, David Pointer, Andrew Splawski January 1, 2010
Application of Sgamma Model with CFD Code to Predict Subcooled Boiling Flow B.J. Yun, A. Splawski, S. Lo, C.–H. Song January 1, 2010
Recent progress in CFD modelling of multiphase flow in horizontal and near-horizontal pipes Simon Lo, Antonino Tomasello January 1, 2010
Predicting pressure drop in pneumatic conveying using the discrete element modelling approach Vikrant Singh, Simon Lo January 1, 2010
Large-Eddy Simulation for an Axisymmetric Piston-Cylinder Assembly With and Without Swirl K. Liu, D. C. Haworth January 1, 2010
ON THE ROLL DAMPING OF AN FPSO WITH RISER BALCONY AND BILGE KEELS R van ’t Veer, F Fathi January 1, 2010
Industrial LES with Unstructured Finite Volumes January 1, 2010
Eulerian-Eulerian CFD Model for the Sedimentation of Spherical Particles in Suspension with High Particle Concentrations B. Balakin, A. Hoffmann, P. Kosinski, L. Rhyne January 1, 2010
Evaluation of One-Group Interfacial Area Transport Equation for the Air/water Flow Condition with CFD Code B.J. Yun, A. Splawski, S. Lo, C.–H. Song January 1, 2010
Design and Optimization of a Fin Stabilizer Using CFD Codes and Optimization Algorithms 1 S. Della Rosa, 2 M. Maceri, 3 I.M. Viola, 4 S. Bartesaghi November 26, 2009
Simulation of Open Channel Turbulent Flow Over Bridge Decks and Formation of Scour Hole Beneath the Bridge Under Flooding Conditions Bishwadipa Adhikary, Pradip Majumdar, Milivoje Kostic, Steven A. Lottes November 13, 2009
Three-dimensional scouring analysis for open channel pressure flow scour under flooded bridge decks Bishwadipa Adhikary, Pradip Majumdar, Milivoje Kostic, Steven A. Lottes, Bhaskar Rao Tulimilli November 13, 2009
Simultaneous Evaluation on Aerodynamics and Air-cooling Performances for Motorcycle using CFD Analysis T. Shimizu, T. Abe, Y. Sunayama, S. Watanabe, E. Nakamura November 3, 2009
Structural and Aerodynamics Analysis on Different Architectures for the Elettra Twin Flyer Prototype P. Gili, M. Battipede, M. Visone, M. Vazzola, P. Farina November 1, 2009
Advances in Simulation for Marine Engineering M. Perić, E. Schreck October 20, 2009
Accuracy and stability in incompressible SPH (ISPH) based on the projection method and a new approach Peter Stansby, Dominique Laurence October 1, 2009
Numerical investigation of supercritical water-cooled nuclear reactor in horizontal rod bundles Zhi Shang, Simon Lo September 30, 2009
STAR-CCM+ and the Orion Launch Abort Vehicle J. Melton September 30, 2009
Flow Induced Vibration Forces on a Fuel Rod by LES CFD Analysis A. M. Elmahdi, R. Lu, M. E. Conner, Z. Karoutas, E. Baglietto September 25, 2009

Pages