Technical Library

Some articles have copyright restrictions,
in order to download these you will be redirected to the copyright holder's website.

 
Name Author(s) Datesort ascending
Numerical Simulation of the Flow Around a Simplified Vehicle Model with Active Flow Control S. Krajnovic, J. Fernandes February 1, 2011
Large Eddy Simulation of the Vortex End in Reverse-Flow Centrifugal Separators G. Pisarev, A. Hoffmann, W. Peng, H. Dijkstra February 1, 2011
Virtual Flow Bench Test of a Two Stroke Engine Andrew Sugden January 5, 2011
Performance of Three-Dimensional Annular Diffusers with Varying Dump Gap Ratios B. C. Bernier, J. Dunn, M. Ricklick, J. Kapat January 4, 2011
Auxiliary Inlet Design Using StarCCM+ Kevin Neitzel January 1, 2011
DEM-CFD simulations of fixed bed reactors with small tube to particle diameter ratios T. Eppinger, K. Seidler, M. Kraume January 1, 2011
Study of the Reverse Delta Wing Afaq Altaf, Ashraf A. Omar, Waqar Asrar, Hani Bin Ludin Jamaluddin January 1, 2011
CFD Analysis of Gas Exchange Process in a Motored Small Two-stroke Engine R. Hariharan, N.V. Mahalakshmi, J. Krishnamoorthy January 1, 2011
On the Approximation of Local Efflux/Influx Bed Discharge in the Shallow Water Equations Based on a Wave Propagation Algorithm H. Mahdizadeh, P. K. Stansby, B. D. Rogers January 1, 2011
An Aerosol Rapid Compression Machine for Studying Energetic-Nanoparticle-Enhanced Combustion of Liquid Fuels C. Allen, G. Mittal, C.J. Sung, E. Toulson, T. Lee January 1, 2011
Coupled Building Pollutant Transport Simulation Tom Chyczewski, Seungbae Hong January 1, 2011
Transported Probability Density Function Methods for Reynolds-Averaged and Large-Eddy Simulations January 1, 2011
Validity of Commercial CFD Codes in Low-Budget Race Car Development J. Ginete, J. Moore, G. Tartaglione January 1, 2011
Development of the Advanced Simulator for Fly Ash Modification in the Pulverized Coal Combustion Furnace O. Akira, S. Akira, T. Tatsumi,, I. Ryunosuke, T. Masato, T. Takahiko January 1, 2011
Numerical Simulation of Fluid Flow and Heat Transfer of Supercritical CO2 in Micro-Porous Media H. S. Choi, H. C. Park, C. Huh, S.G. Kang January 1, 2011
Computational Investigation of Water Dynamics in a PEM Fuel Cell Cathode Channel M. Hossain December 17, 2010
Simulation of Flow Around KCS-Hull S. Enger, M. Perić, R. Perić December 8, 2010
Practical CFD to Compute Resistance, Sink and Trim of Fully Appended Sailing Yachts I. M. Viola, R.G.J. Flay December 5, 2010
The Effects of Injection Timing and Piston Bowl Shape on PHCCI Combustion with Split injections Sangyul Lee, Hoimyoung Choi, Jaewoo Chung December 4, 2010
Simulated elliptical bioprosthetic valve deformation: Implications for asymmetric transcatheter valve deployment Wei Sun, Kewei Li, Eric Sirois December 1, 2010
Progress in the Self-Similar Turbulent Flame Premixed Combustion Model V. Moreau December 1, 2010
Computational Evaluation of Platelet Activation Induced by a Bioprosthetic Heart Valve Eric Sirois, Wei Sun November 18, 2010
Large Eddy Simulation for thermal fatigue prediction in a T-Junction :Wall function or Wall-resolve based LES S.T. Jayaraju, E.M.J. Komen, E. Baglietto November 1, 2010
STAR-CCM+ Boiling Model Validation Dr. Emilio Baglietto November 1, 2010
Multiphase CFD-CHT Analysis and Optimization of the Cooling Jacket in a V6 Diesel Engine S. Fontanesi, G. Cicalese, M. Giacopini October 25, 2010
Efficient CFD Simulation Process for Aeroacoustic Driven Design F. Mendonça, A. Read, F. Imada, V. Girardi October 17, 2010
Efficient CFD Simulation Process for Aeroacoustic Driven Design Fred Mendonça, Alex Read, Fabiano Imada, Vinicius Girardi October 17, 2010
Comparison of the stochastic fields method and DQMoM-IEM as turbulent reaction closures Jethro Akroyd, Alastair J. Smith, Laurence R. McGlashan, Markus Kraft October 15, 2010
CFD Analysis of a Duct’s Effectiveness for Model Scale and Full Scale Tobias Zorn, Justus Heimann, Volker Bertram October 10, 2010
CFD Simulation of Orifice Flow for the Flooding of Damaged Ships Christian D Wood, Dominic A Hudson, Mingyi Tan October 10, 2010
CFD validation of different propeller ducts on open water condition Alejandro Caldas, Marcos Meis, Adrián Sarasquete October 10, 2010
Using CFD for simulation of ships with different fuel saving rudder-propeller devices Claus D. Simonsen, Christian Klimt Nielsen, Zdravko Kishev October 10, 2010
CFD optimization of vortex generators forming the wake flow of large ship Pawel Dymarski, Marek Kraskowski October 10, 2010
Computational Evaluation of the Performance of Lifting Surfaces with Leading-Edge Protuberances Paul W. Weber, Laurens E. Howle, Mark M. Murray , David S. Miklosovic October 8, 2010
Aerodynamic and structural design of a plastic sump guard component Bernardo Coelho, Vinicius Leal, Guilherme Carneiro, Jonathan Rodrigues, Nelson Timponi, Thiago Zolet, Glauber Resende October 6, 2010
Direct Injection and Spark Controlled Jet Ignition to Convert A Diesel Truck Engine to LPG A. Boretti October 5, 2010
Computational and Experimental Investigations of Performance Curve of an Axial Flow Fan Using Downstream Flow Resistance Method S. H. Liu, R. F. Huang, C. A. Lin October 1, 2010
Aneurysm Inflow-Angle as a Discriminant for Rupture in Sidewall Cerebral Aneurysms Morphometric and Computational Fluid Dynamic Analysis Merih I. Baharoglu, Clemens M. Schirmer, Daniel A. Hoit, Bu-Lang Gao, Adel M. Malek October 1, 2010
Film Thickness Prediction in an Annular Two-Phase Flow Through Bends P. M. Tkaczyk, H. P. Morvan September 30, 2010
A Multi-Disciplinary Approach for Design Improvement of an Air-Cooled Two-Wheeler Engine Cylinder Head Om Singh, T. Sreenivasulu, M. Kannan, K. Nagaraja September 28, 2010
Computational Analysis of Flow Structure and Particle Deposition in a Single Asthmatic Human Airway Bifurcation H. Zhang, G. Papadakis September 17, 2010
CFD in Supercritical Water-Cooled Nuclear Reactor (SCWR) with Horizontal Tube Bundles Z. Shang, S. Lo September 1, 2010
CFD Methodology and Validation for Single-Phase Flow in PWR Fuel Assemblies M. Conner, E. Baglietto, A. Elmahdi September 1, 2010
EVALUATION OF AN EXPERIMENTAL DATA SET TO BE VALIDATION DATA FOR CFD FOR A VHTR Richard W. Johnson September 1, 2010
Studies Related to the Oregon State University High Temperature Test Facility: Scaling, the Validation Matrix, and Similarities to the Modular High Temperature Gas-Cooled Reactor Richard R. Schultz, Paul D. Bayless, Richard W. Johnson, Glenn E. McCreery, William Taitano, James R. Wolf September 1, 2010
Effect of Process Conditions on Dynamics and Performance of PEMFC: Comparison With Experiments H. Y. Park, J. W. Hwang, K. T. Park, S. Kim, Y. U. Jeong, H. W. Jung, S. H. Kim September 1, 2010
Modeling of flame lift-off length in diesel low-temperature combustion with multi-dimensional CFD based on the flame surface density and extinction concept Ulugbek Azimova, Ki-Seong Kima and Choongsik Baeb September 1, 2010
Computation of Wall-Pressure Spectra from Steady Flow Data for Noise Prediction S. Remmler, J. Christophe, J. Anthoine, S. Moreau September 1, 2010
CFD applied to super and mega yatch design R Azcueta, N Rousselon August 18, 2010
Distribution and Magnitude of Shear Stress after Coronary Bifurcation Lesions Stenting with the Classical Crush Technique: A New Predictor for In-Stent Restenosis Z.H. Hu, S.L. Chen, J.J. Zhang, S.J. Shan, Z.Z. Liu, F. Ye, J. Kan, H.M. Xu, K. Nguyen, T. Kwan, T. Nguyen, T. Hoang August 1, 2010

Pages