Technical Library

Some articles have copyright restrictions,
in order to download these you will be redirected to the copyright holder's website.

 
Namesort descending Author(s) Date
Aerospace Applications & Case Studies Deryl Snyder
After treatment :SCR modeling using STAR-CCM+ Richard Johns
Air-Gap Convection in a Switched Reluctance Machine Pietro Romanazzi, David A. Howey November 25, 2015
Aircraft Damping Derivative Estimation Using STAR‐CCM+ Angelo Lerro
Aircraft Damping Derivatives Estimation Using STAR-CCM+ A. Lerro, M. Visone
Aircraft Passenger Cabin Thermal Comfort Analysis D. Cannoletta
Aircraft Passenger Cabin Thermal Comfort Analysis by Means of Integrated Mono Dimensional/CFD Approach P. Borrelli, A. Romano, D. Cannoletta
Airflow Analysis of a Custom “Green” Air Handling Unit Without a Pre-heater Scott Reynolds
Alternative fuels for IC Engines Andreas Kolbeck
An Aerosol Rapid Compression Machine for Studying Energetic-Nanoparticle-Enhanced Combustion of Liquid Fuels C. Allen, G. Mittal, C.J. Sung, E. Toulson, T. Lee January 1, 2011
An experimental and modelling approach to the determination of auto-ignition of diesel fuel, dodecane and hexadecane sprays at high pressure Alvaro Diez, Terese Løvås, Roy J. Crookes May 9, 2013
An Innovative Transient Post-Processing Approach for a Full Car Thermal Validation Study Yves-Marie Lefebvre, Lester DeLeon, Sachin Badarayani
An integrated approach for simulating diesel engine performance using Direct Injection Stochastic Reactor Model (DI-SRM) Michal Pasternak, Andrea Matrisciano
An Investigation of the Impact of the Proton Exchange Membrane Fuel Cell Flow Field Plate Geometry and Design Using Computational Fluid Dynamic Modeling and Simulation Vijay Edupuganti , Dr. Bevin Daglen February 21, 2012
An Investigative Study of Microfluidic Capabilities of STAR-CCM+ Harpreet S. Matharoo July 31, 2013
An overview of battery simulation Robert Spotnitz
An Overview of CFD Applications in Flow Assurances from Well Head to the Platform Simon Lo
Análisis del diseño de la carrocería de un coche tipo Fórmula Julio César Pérez Aguilar January 1, 2015
Analysis & Modeling in CFD of the Mixing in an Industrial Anaerobic Membrane Bioreactor Jorge López
Analysis of Asymmetric Aircraft Aerodynamics Due to an Experimental Wing Glove Fletcher Hartshorn June 27, 2011
Analysis of Flow Induced Noise in a Passenger Car Exhaust System - An Experimental and Numerical Approach D. Rana, F. Regin, M. Makana May 17, 2011
Analysis of GDL flooding effects on PEMFC performance S. Shimpalee , U. Beuscher, J.W. Van Zee August 1, 2007
Analysis of Scarfed Shape Effect over Slab Heating Process Jun-Seok Lim , Hyeong-Jin Kim , Hyun-Joon Kim
Analysis of the 3D Flow & Heat Transfer of the Finned-Tube Bank for Creation Effective Counting Method for Steam Turbines Oil Coolers Yulia S. Bagaeva, N. N. Kortikov
Analysis of the airstream in the ECS roller dynamometer building Stefan Schnörch
Analysis of the Coffee Roasting Process under Actual Operating Conditions Stefano Farina, Massimo Milani, Luca Montorsi
Analysis of the Corrosion Test Process for Heat Exchangers in Corrosion Test Chambers by CFD Simulation Rainer Stauch, F. Brändle, M. Pfitzer, Wolfram Kühnel
ANALYSIS OF THE INTERFACIAL AREA TRANSPORT MODEL FOR INDUSTRIAL 2-PHASE BOILING FLOW APPLICATIONS K. Goodheart, N. Alleborn, A. Chatelain and T. Keheley May 12, 2013
Analysis of the Lubrication System in a High Pressure Piston Water Pump Davide Bottazzi, D. Galloni, M. Milani, L. Montorsi
Analysis of two-phase flows in pipes and subchannels under high pressure N. Alleborn, R. Reinders, S. Lo, A. Splawski
Analysis of Void Fraction Distribution and Departure from Nucleate Boiling in Single Subchannel and Bundle Geometries Using Subchannel, System, and Computational Fluid Dynamics Codes Taewan Kim , Victor Petrov, Annalisa Manera, Simon Lo July 20, 2012
ANALYTICAL SCALING OF DEM PARTICLES FOR EFFICIENT PACKED-BED SIMULATIONS Ricklick, M, Baran, O July 14, 2014
Analyzing Local Combustion Environment with a Flamelet Model and Detailed Chemistry Ossi Kaario, Armin Wehrfritz, Martti Larmi, Anders Brink April 1, 2012
Aneurysm Inflow-Angle as a Discriminant for Rupture in Sidewall Cerebral Aneurysms Morphometric and Computational Fluid Dynamic Analysis Merih I. Baharoglu, Clemens M. Schirmer, Daniel A. Hoit, Bu-Lang Gao, Adel M. Malek October 1, 2010
Annual Building Energy Simulation with STAR-CCM+ Tunc Askan & Martin Kriegel
Application of CFD in connection with ship design Claus Daniel Simonsen
Application of computational fluid dynamics to spray drying Simon LO July 5, 2005
Application of DARS 1D on in-cylinder combustion and aftertreatment Karin Fröjd
Application of DEM Model of STAR-CCM+ for Granular Flow Through a Pipe 加藤 丈侍様
Application of Direct Quadrature Method of Moments in Multiphase Flows using STAR-CCM+ John Parra-Alvarez
APPLICATION OF MAGNETOCALORIC EFFECT IN THE DESIGN OF EFFICIENT REFRIGERATION SYSTEM S. P. VENDAN, D. DINESH, A. GIRISH January 1, 2009
Application of Sgamma Model with CFD Code to Predict Subcooled Boiling Flow B.J. Yun, A. Splawski, S. Lo, C.–H. Song January 1, 2010
Application of STAR-CCM+ in Marine & Off-Shore Engineering: State-of-the-Art & New Developments Eberhard Schreck, Frank Schaefer, Jaswinder Singh, Milovan Peric
Application of STAR-CCM+ to Turbocharger Modeling at BorgWarner Turbo Systems David Grabowska, Dean Palfreyman, Bob Reynolds, Fred Mendonca
Application of STAR-CCM+ to turbocharger performance prediction: A Power train perspective Fred Mendonca
Application of Sweep to Low Pressure Turbine Cascade Blade for Tip Flow Containment Rachel F. Trehan1 and Bhaskar Roy² July 15, 2012
Applications of Large Eddy Simulations in Nuclear Field J.P. Simoneau, J. Champigny, O. Gelineau February 1, 2010
Applications of Overset Mesh Technique for the Marine Industry Hans Jorgen Morch
Applied CFD Education using STAR-CCM+ Sean Sloan
Approaches for Acoustics Simulation for Automotive Air Induction & Exhaust Systems Fabiano Bet, Gerald Seider, Simon Bless

Pages