Technical Library

Some articles have copyright restrictions,
in order to download these you will be redirected to the copyright holder's website.

 
Namesort descending Author(s) Date
Numerical and Experimental Study of Deposition of Polystyrene Particles in Multiphase Pipe Flows Fasil Ayelegn TASSEW June 1, 2015
Numerical Evaluation of Averaging BDFT(bidirectional flow tube) Flow meter on Applicability in the Fouling Condition Jong-Pil Park
Numerical Investigation of Diameter Effect on Heat Transfer of Supercritical Water Flows in Horizontal Round Tubes Z. Shang, S. Chen March 1, 2011
Numerical investigation of DQMoM-IEM as a turbulent reaction closure Jethro Akroyd, Alastair J. Smith, Laurence R. McGlashan, Markus Kraft March 15, 2010
NUMERICAL INVESTIGATION OF HEAT AND MASS TRANSFER IN A REFRIGERATED TRUCK COMPARTMENT T. LAFAYE DE MICHEAUX, V. SARTRE, A. STUMPF, J. BONJOUR January 1, 2013
Numerical investigation of supercritical water-cooled nuclear reactor in horizontal rod bundles Zhi Shang, Simon Lo September 30, 2009
Numerical investigation of the effect of bed height on minimum fluidization velocity of cylindrical fluidized bed Ajay M R, Aditya Karnik December 10, 2012
Numerical Investigation of the Effect of Bed Height on Minimum Fluidization Velocity of Cylindrical Fluidized Bed Ajay M R July 31, 2013
Numerical Investigation on Performance & Emission Characteristics of CI & SI Engine using 1D Cycle Simulation & DOE Method Jungsoo Park
NUMERICAL INVESTIGATIONS OF WIND TURBINES ON A SLANTED WALL Shahab Moayedian, Hamid Rahai November 11, 2011
Numerical Investigations on Methods to Control the Rate of Heat Release of HCCI Combustion Using Reduced Mechanism of N-Heptane With a Multidimensional CFD Code F. Maroteaux, L. Noel, A. Ahmed January 1, 2007
NUMERICAL INVESTIGATIONS ON THE NOISE CHARACTERISTICS OF A RADIAL FAN WITH FORWARD CURVED BLADES Manoochehr DARVISH, Stefan FRANK December 2, 2012
Numerical Investigations on the Performance Characteristic of Radial Fans with Forward Curved Blades by means of CFD Manoochehr Darvish
Numerical Investigations on the Performance Characteristic of Sirocco Fans by Means of Computational Fluid Dynamics M. Darvish, S. Frank
Numerical Modeling of Resistance for a Conceptual Seatrain N. Harpal, C. Patel March 31, 2011
Numerical Modeling of Ship Propeller Interaction under Self-Propulsion Condition Vladimir Krasilnikov
Numerical Modelling of Cavitation: Validation and Parametric Studies X. Margot, S. Hoyas, A. Gil , S. Patouna March 1, 2012
Numerical Modelling of Ship Stern Flows P. L. Nielsen January 1, 2007
Numerical Modelling of the Flow Around the Tanker Hull at Model Scale Boris Bućan, Marta Pedišić Buča, Stanislav Ružić June 1, 2008
Numerical Predictions of Gas Porosity in Casting Processes using Fully Coupled Mold-filling and Solidification Simulation S. Jana, J. Jakumeit, M. Y. Jouani June 7, 2009
Numerical simulation and wind tunnel measurements on a tricycle wheel sub-system Thomas Driant, Lakhdar Remaki, Stéphane Moreau, Alain Desrochers, Hachimi Fellouah March 26, 2012
Numerical Simulation for Ignitability of Spark Plug Using In-Cylinder Combustion Model 吉崎 博俊様
Numerical simulation in vertical wind axis turbine with pitch controlled blades Bayeul Annie-Claude, Dockter Aurore, Simonet Sophie, Bois Gérard
Numerical Simulation of a Hydrocarbon Fuelled Valveless Pulse Jet Joseph Kalyan Raj Isac, Logu M July 31, 2013
Numerical Simulation of Airflow around Horizontal Axis Wind Turbine
Numerical Simulation of DLR-F11 High Lift Configuration using STAR-CCM+ Prashanth Shankara, Jeremy Hanke & Deryl Snyder
Numerical Simulation of Flow Field Formed in Water-Pump Sump Annie-Claude Bayeul-Lainé, Gérard Bois, Abir Issa
Numerical Simulation of Fluid Flow and Heat Transfer of Supercritical CO2 in Micro-Porous Media H. S. Choi, H. C. Park, C. Huh, S.G. Kang January 1, 2011
Numerical Simulation of Friction Stir Butt Welding Process for AA5083-H18 Sheets D. Kim, H. Badarinarayan, J. H. Kim,, C. Kim, K. Okamoto, R.H. Wagoner, K. Chung March 1, 2010
Numerical simulation of particle soiling in the engine compartment of a bus SIMON LINDBERG January 1, 2015
Numerical Simulation of the air flow around an tractor-trailer configuration with realistic areodynamic conditions and comparison to experimental data from a road test Henri Karhula May 30, 2013
Numerical Simulation of the Flow Around a Simplified Vehicle Model with Active Flow Control S. Krajnovic, J. Fernandes February 1, 2011
Numerical simulation of the flow in wire-wrapped pin bundles: Effect of pin-wire contact modeling E. Merzari, W.D. Pointer, J.G. Smith, A. Tentner, P. Fischer October 13, 2011
Numerical Simulation of Unsteady Interaction of Hot Streams with HPT Rotor Blades using Harmonic Balance Method Implemented in STAR-CCM+ A.I. Iakunin, N.B. Kuznetcov, A.E. Tcvetaev
Numerical simulations of high temperature jets from the main propulsion system and auxiliary power unit impinging against a construction of the passenger plane Andrey Y. Kudryaytsev, S.A. Zhelezov, M.M. Polovin, M.S. Litvinov
Numerical simulations of the sails aerodynamics for a 16th century Portuguese nau COSMIN CIORTAN, NUNO FONSECA September 28, 2011
Numerical studies on rib&channel dimension of flow-field on PEMFC performance S. Shimpalee, J.W. Van Zee May 1, 2007
Numerical study of cavitating flow inside a flush valve Annie-Claude BAYEUL-LAINẺ, Sophie SIMONET, Guy CAIGNAERT
Numerical study of flow stream in mini wawt with relative rotating blades Bayeul Annie-Claude, Simonet Sophie, Dockter Aurore, Bois Gérard
Numerical Study of Pressure Waves Using Finite Volumes Method C. Falcao, S. Hanriot, H. Vielmo May 16, 2013
Numerical Validation of the Noise Characteristics of the Radial Fans with Forward Curved Blades Manoochehr Darvish
Numerische Simulation der Hydrodynamik, des Stoffumsatzes und der chemischen Reaktion in einem T-förmigen Mikromischer Fabian Huck September 16, 2011
Numerische Simulation zur Ermittlung und Optimierung des durch Windströmung induzierten Schwingungsverhaltens der StRailer-Fahrzeugkabine Christian Bulut November 30, 2011
Numerische Strömungssimulation zur Berechnung der Verweilzeitverteilung in einem Biogasreaktor Christian Bock November 28, 2011
Numerische Untersuchung des Wärmeübergangs an Rotoroberächen elektrischer Maschinen unter Nutzung des Injektionsprinzips Christian Franz March 24, 2015
Observation & CFD Analysis of Steady/Unsteady Natural Convection Phenomena in a Room with Floor Heating 酒井 孝司様
OMAE 2012 -83472: Offshore Platform FSI Simulation C.S.
On the Aerodynamics of Car Body Vibrations of High-Speed Trains Cruising Inside Tunnels B. Diedrichs, S. Krajnovic January 1, 2008
On the Approximation of Local Efflux/Influx Bed Discharge in the Shallow Water Equations Based on a Wave Propagation Algorithm H. Mahdizadeh, P. K. Stansby, B. D. Rogers January 1, 2011
On the development of a full-scale numerical towing tank Reynolds scaling effects on ducted propellers and wakefields Norbert Bulten, Maarten Nijland June 1, 2011

Pages