Technical Library

Some articles have copyright restrictions,
in order to download these you will be redirected to the copyright holder's website.

 
Name Author(s) Datesort ascending
Fluid/Thermal Modeling of a LOX/Propylene Thruster with Radiative and Fuel Film Cooling Glen Guzik July 31, 2013
Optimization of Under-Relaxation Factors and Courant Numbers for the Simulation of Sloshing in the Oil Pan of an Automobile Swathi Satish, Mani Prithiviraj, Sridhar Hari July 31, 2013
Numerical Simulation of a Hydrocarbon Fuelled Valveless Pulse Jet Joseph Kalyan Raj Isac, Logu M July 31, 2013
CDF code validation of rotor/fuselage interaction using the commercial software STAR-CCM+8.04 Boris Kubrak, Deryl Snyder July 1, 2013
Stroemungsanalyse um ein Formula-Student-Auto mittels CFD Karl Hantschmann, Christopher Horlebein June 21, 2013
Optimierung um ein Formula-Student-Auto mittels TOSCA-Fluid Christopher Horlebein, Karl Hantschmann June 21, 2013
INVESTIGATION OF TURBINE CASCADE BLADES WITH PART-SPAN SWEEP WITH AN OPEN END Rachel Trehan and Bhaskar Roy June 3, 2013
UNSTEADY SIMULATION OF A TWO-STAGE COOLED HIGH PRESSURE TURBINE USING AN EFFICIENT NON-LINEAR HARMONIC BALANCE METHOD Chad H. Custer, Jonathan M. Weiss, Venkataramanan Subramanian, Kenneth C. Hall June 3, 2013
Numerical Simulation of the air flow around an tractor-trailer configuration with realistic areodynamic conditions and comparison to experimental data from a road test Henri Karhula May 30, 2013
Prediction of a subcooled boiling flow with advanced two-phase flow models Byong-Jo Yun, Andrew Splawski, Simon Lo, Chul-Hwa Song May 21, 2013
Interaction of Multiple Fuel Sprays in a Heavy-Duty Diesel Engine Armin Wehrfritz, Ossi Kaario, Ville Vuorinen, Aki Tilli, Martti Larmi May 16, 2013
Numerical Study of Pressure Waves Using Finite Volumes Method C. Falcao, S. Hanriot, H. Vielmo May 16, 2013
Fluid Structure Interaction Using Small Displacement Theory CD-adapco May 16, 2013
Influences of Free Stream Conditions on Vehicle Thermal Management – An Analytical Study K. T. Lan, K. Srinivasan May 16, 2013
ANALYSIS OF THE INTERFACIAL AREA TRANSPORT MODEL FOR INDUSTRIAL 2-PHASE BOILING FLOW APPLICATIONS K. Goodheart, N. Alleborn, A. Chatelain and T. Keheley May 12, 2013
An experimental and modelling approach to the determination of auto-ignition of diesel fuel, dodecane and hexadecane sprays at high pressure Alvaro Diez, Terese Løvås, Roy J. Crookes May 9, 2013
CFD Methodology to Correlate the Defrost Flow and Passenger Car's Windshield Defogging T. L. Zolet, G. F. de Reitas Maia, G. G. Dutra, L. V. Mendes Pereira May 9, 2013
A study of the losses and interaction between one or more bow thrusters and a catamaran hull L Boddy , T Clarke May 7, 2013
Design and Simulation of Spirally-Wound Lithium-Ion Cells Robert Spotnitz, Steve Hartridge, Gaetan Damblanc, Gowri Yeduveka, Donald Schad, Venugopal Gudimetla, Jeffery Votteler, Gene Poole, Chris Lueth, Christian Walchshofer, Evan Oxenham April 25, 2013
Untersuchung des Wärmeabtransports an einem im EETNEK PV-Outdoor-Labor eingebundenen PV-Moduls mittels eines numerischen Simulationsmodells Thomas Basten April 15, 2013
Direct numerical simulation of pore-scale flow in a bead pack: Comparison with magnetic resonance imaging observations Xiaofan Yang a, Timothy D. Scheibe a,⇑, Marshall C. Richmond a, William A. Perkins a, Sarah J. Vogt b, Sarah L. Codd c, Joseph D. Seymour b, Matthew I. McKinley a February 27, 2013
Parametric B-Wagenigen screw model. Verify compliance CFD computation with hydrodynamics plots Andrzej Rachwalik February 18, 2013
Windkraftanlagen mit vertikaler Achse (VAWT): Der C-Rotor im Windkanalversuch und Strömungssimulation in STAR-CCM+ Felix Furtmayr February 18, 2013
NUMERICAL INVESTIGATION OF HEAT AND MASS TRANSFER IN A REFRIGERATED TRUCK COMPARTMENT T. LAFAYE DE MICHEAUX, V. SARTRE, A. STUMPF, J. BONJOUR January 1, 2013
THREE DIMENSIONAL CFD SIMULATION OF A TURBOCHARGER TURBINE FOR MOTORSPORT APPLICATIONS CRISTIAN CAPILUPPI December 27, 2012
THREE DIMENSIONAL CFD SIMULATION OF A TURBOCHARGER TURBINE FOR MOTORSPORT APPLICATIONS Cristian Capiluppi December 27, 2012
Flow Due to Multiple Jets Downstream of a Barrage: Experiments and 3D CFD Modelling using STAR-CCM+ Penny Jeffcoate, Peter Stansby, David Apsley December 18, 2012
DNS of Buoyancy Driven Flow Inside a Horizontal Coaxial Cylinder Imama Zaidi 1, Yacine Addad2, Dominique Laurence1 December 18, 2012
Comparison of predictions obtained on an exhaust manifold analysis using conformal and indirect mapped interface Swathi Satish, Mani Prithiviraj , Sridhar Hari December 11, 2012
CFD PREDICTIONS OF SOLIDS DISTRIBUTION IN STIRRED VESSEL Dominik KUBICKI and Simon LO December 10, 2012
Slurry transport in a pipeline – Comparison of CFD and DEM models Dominik KUBICKI and Simon LO December 10, 2012
Numerical investigation of the effect of bed height on minimum fluidization velocity of cylindrical fluidized bed Ajay M R, Aditya Karnik December 10, 2012
NUMERICAL INVESTIGATIONS ON THE NOISE CHARACTERISTICS OF A RADIAL FAN WITH FORWARD CURVED BLADES Manoochehr DARVISH, Stefan FRANK December 2, 2012
A validation study of lithium-ion cell constant c-rate discharge simulation with Battery Design Studio Apurba Sakti, Jeremy J. Michalek, Sang-Eun Chun, Jay F. Whitcare November 6, 2012
CFD based investigation of potential power saving for different rudder types, positions and pre-swirl fins Claus D. Simonsen, Casper Nielsen, Christian Klimt-Møllenbach, Christian Råe Holm, Anton Minchev November 1, 2012
Counteracting ring formation in rotary kilns M Pisaroni, R Sadi, D Lahaye October 24, 2012
Aerodynamic Investigation of Gap Treatment- and Chassis Skirts Strategies for a Novel Long-Haul Vehicle Combination Helena Martini, Björn Bergqvist, Linus Hjelm, Lennart Lofdahl October 2, 2012
Thermal Modeling of NUHOMS HSM-15 and HSM-1 Storage Modules at Calvert Cliffs Nuclear Power Station ISFSI SR Suffield, JM Cuta, JA Fort, BA Collins,HE Adkins and ER Siciliano October 1, 2012
Irrigation of human prepared root canal – ex vivo based computational fluid dynamics analysis Damir Šnjarić, Zoran Čarija, Alen Braut, Adelaida Halaji, Maja Kovačević, Davor Kuiš October 1, 2012
Aerodynamic analysis and optimisation of the rear wing of a WRC car Eduardo Cañada September 27, 2012
Coupled Computational Fluid Dynamics and MOC Neutronic Simulations of Westinghouse PWR Fuel Assemblies with Grid Spacers Jin Yan, Brendan Kochunas, Mathieu Hursin, Thomas Downar, Zeses Karoutas, Emilio Baglietto September 25, 2012
CFD Modelling of a Biomass Incinerator for Prediction of Risk Areas for Corrosion Damages Svend Skovgaard Petersen September 1, 2012
CFD modeling of boiling flow in PSBT 5x5 bundle Simon Lo, Joseph Osman September 1, 2012
Flow Analysis of Apache Wingsuit Karl Nyberg September 1, 2012
Analysis of Void Fraction Distribution and Departure from Nucleate Boiling in Single Subchannel and Bundle Geometries Using Subchannel, System, and Computational Fluid Dynamics Codes Taewan Kim , Victor Petrov, Annalisa Manera, Simon Lo July 20, 2012
Application of Sweep to Low Pressure Turbine Cascade Blade for Tip Flow Containment Rachel F. Trehan1 and Bhaskar Roy² July 15, 2012
Modelling of heat transfer and solidification processes in horizontal twin-roll casting of magnesium AZ31 A.Miehe , U.Gross July 2, 2012
STAR-CCM+ and SPEED for electric machine cooling analysis Dr. Markus Anders, Dr. Stefan Holst June 26, 2012
Numerical Simulation of High Lift Trap Wing using STAR-CCM+ Prashanth Shankara and Deryl Snyder June 25, 2012
Use of CFD to study Hydrodynamic Loads on Free-Fall Lifeboats in the Impact Phase Stian Ripegutu Johannessen June 1, 2012

Pages