Design & Evaluation of a Passive Micromixer with Curved Shape Obstacles & Grooves in the Mixing Channel

Printer-friendly versionPDF version

Micromixers are key components in several micro electro-mechanical and lab-on-a-chip systems, which are increasingly applied in fields such as chemistry, chemical synthesis, bio-technology and environment control.

A CFD-based study is presented, which includes design modeling, flow and mass transfer simulation and geometric parametric analysis of a passive micromixer that presents curved shape obstacles and grooves in the mixing channel as main geometric features. The parametric study helps to identify the effect of some geometric dimensions on mixing quality, pressure loss and shear stress levels. The aim of the study is to reduce the pressure drop while keeping the mixing level in the channel with the inclusion of grooves which create additional secondary flows in a chaotic pattern and reduce the effect of the nozzle formed at the tip of the obstacles. 

To our knowledge, this specific combination of obstacles and grooves in micromixer geometries has not been previously investigated.

Author Company: 
University of Hertfordshire
Author Name: 
Cesar Augusto Cortes-Quiroz, Mark Tracey
Products: