Library

2928 match your search

STAR-CCM+ v11.06 新機能紹介ウェビナー
本ウェビナーでは、 2016年10月26日に世界同時リリースされたSTAR- CCM+ v11.06の 新 機能 情報について、 下記の 機能 を中心にご 紹介 いたします。 最 新 バージョン v11.06では、v11のテーマである、“ Discover Better Designs, Faster. ”(より良い設計をより早く見つけ出す) に基づき、電子機器冷却ツールセット(E-Cool) の導入をはじめ、主として以下の 機能 追加・ 機能 改良を行っています。 ・E-Cool 電子機器冷却用解析ツールセットE- Coolが 新 しく追加されました。ファン、 ヒートシンクなどの形状作成から熱性能評価までの一貫した解析が できるようになります ・シミュレーションツリー比較 機能 これまで困難であったシミュレーションの設定の違いを簡単に識別 できるようになります ・パーツベースの押出しメッシャー これまでメッシュ連続体でしか利用できなかった押出しメッシャー がパーツベースメッシュでも実施可能になります ・局所サーフェスラッパー 局所的にラッピングサーフェスを生成することにより、 メッシュ生成にかかる時間を大幅に短縮できるようになります ・適応型混合粒径群ポピュレーションバランスモデル(A-MUSIG) 分散相の集合挙動を正確に予測する 新 しいモデルが搭載されました 。...
Redução de custo através de Simulações de Engenharia para a Indústria de Processos e Manipulação de Materiais
Engenharia hoje é uma realidade para todos os parques industriais do país. A engenharia inovadora e de alta tecnologia é uma necessidade para aumentar a competitividade e reduzir custos em um mercado desafiador. Inovação e tecnologia na engenharia é necessário para a empresa manter competitividade, mas não por isto precisa ser algo complexo e caro de ser aplicado. O que tem em comum as indústrias de processos, tais como Papel e Celulose, Químicas, Farmacêutica, Mineração, Grãos, Alimentícia? Todas possuem equipamentos de mistura de materiais sólidos e/ou fluidos, além de equipamentos de...
You’ve been there; we’ve all been there. Can’t sleep in the early morning hours, turn on the TV and bam, there’s an infomercial that touts a product as the do-everything solution you’ve been waiting for your entire life. This isn’t an infomercial. And we’re not offering something that will turn off your lights before you jump into bed or teleport you home ahead of rush hour traffic. But this is something that, as a process engineer, will make your life a whole lot easier. Admixtus is a Virtual Product Development Tool that seamlessly integrates with our industry-leading engineering simulation software tool STAR-CCM+® to create geometries, set up CFD simulations, and carry out analysis of stirred vessels. Admixtus automates your workflow to set up a simulation from CAD geometry to analysis in a few simple steps. Pretty cool, right? Even better, Admixtus is a great tool for students to learn about mixing in industrial scale systems. Perhaps best of all, Admixtus does not have any additional costs associated with it. Check out more on Admixtus and how it can change your engineering life by helping you overcome annoying design hurdles by registering for our upcoming complimentary global webinar, “Admixtus is the time and cost saving solution for process development engineers” to be held on December 9, 2016.The webinar will also cover multiphysics aspects such as using Discrete Element Modeling (DEM) for solids suspension, Fluid Structure Interaction (FSI) and modeling reactions in the fermentation process.
Don’t worry, this blog has nothing to do with politics. Instead I wanted to spend some time trying to understand the lessons that we as engineers can learn from the failure of the prediction community to successfully forecast the outcome of the 2016 Presidential Election. For me this was an important backstory to the 2016 campaign: the pre-election poll predictions were wrong by a significant enough margin that they completely failed to forecast the outcome of the election. “What does this have do with engineering simulation?” I hear you ask. The answer, I think, is “a great deal.” CFD engineers, like psephologists*, are also interested in making predictions about the future. Whereas Silver and his peers use statistical inference (from opinion polls and other data sources) to try and predict how people will vote in an election, we use numerical models of physics to predict the future performance of a proposed product or design.
If you pack too much matter into a small space, you are likely to get some undesirable consequences as anyone vacationing with small kids will be all too aware. If you have to sit on your suitcase to get it closed, you are likely to be greeted by the sight of your holiday clothes circling on the carousel at your destination. Similar consequences befall the engineer simulating two-way coupled fluid-particle systems when they overload cells in the CFD mesh with too much DEM matter. I refer, of course, to the previous requirement that a DEM particle must be smaller than the flow cell it occupies for two-way coupled simulations. This limitation is due to the way the effects of the DEM particle are applied purely to the flow cell in which the particle centroid lies, and not to adjacent cells that are also overlapped by the particle. When DEM particles are larger than the cell, this results in large sources of momentum and energy being applied to individual cells causing instability and divergence. However, it is not just stability that can be compromised, but also accuracy, with the void fraction of the particle not being fully accounted for if the volume of the cell is smaller than the particle. In practice, this rendered some applications impossible to simulate as geometrical features forced the mesh size to be smaller than particles. The recent release of STAR-CCM+® v11.06 changes all that with DEM source smoothing…
Designing ships for future challenges – a paradigm shift in vessel design
To many companies within the marine industry, it is becoming clear that the combined effect of tackling climate change and the increasingly competitive market landscape requires new and innovative products and business models to be delivered at an ever-increasing pace if they are to survive and secure long-term prosperity. Amplified by the downturn in oil prices and the global economy, companies – both new and old – find success or failure based on how they adapt and respond to these circumstances. This webinar will demonstrate how using simulation in new and deliberate ways is helping...
Look around your desk, within reach of you right now. How many things do you see that have a circuit board, a couple of chips and maybe an LED or two in them? I count 12, and that’s just within reach. When you think about the electrification of our world, smaller, more powerful and newest are the three words that describe the value of a piece of electronics. So let’s look at these two statements through the eyes of a typical thermal analyst: “I have to build and analyze, smaller, hotter and faster to stay competitive.” That is precisely the reason we have spent the last few years developing the Electronics Cooling Toolset within STAR-CCM+® software. We recognized that designers in the electronics market need tools to setup, run and analyze their products in STAR-CCM+ but with fewer clicks, more interactivity, and a much more focused interface. This is a tool available to every user, aptly named the Electronic Cooling Toolset, or E-cool for short.
Advancements for in-cylinder analysis and design exploration
STAR-CD ® /es-ice/DARS is a market-leading toolset for in-cylinder CFD simulations that offers the most advanced physical models for combustion and emissions formation. Furthermore, combining such a toolset with design space exploration enables the discovery of more innovative designs to help maximize fuel economy and performance while minimizing the formation of harmful pollutants. View this On-Demand Webinar to get up to speed on the latest developments for the Siemens PLM Software in-cylinder solution and learn how to get better combustion system designs, faster. Topics covered will...
Imagine finally picking up your new Tesla after months of waiting (popular cars have waiting lists). While counting down the days, you daydream about driving that beauty on the freeways and cruising downtown as the commoners turn their heads to catch a glimpse. The last thing you are going to worry about is if the battery is defective or even ineffective. Yet while often overlooked, the battery is arguably the most important part of the vehicle. But don’t worry; chances are that well before you placed your order, computer-aided engineering (CAE) was used to ensure that the battery of your amazing new car will let you feel like Batman and not a Joker.
From overheating phones to underperforming data centers, thermal malfunction of electronics devices is not just a nuisance but a performance and safety risk. It is no secret then that thermal reliability is at the forefront of an electronics engineer’s design concerns. Demand for high power density devices in smaller packaging requires innovative cooling strategies. Traditional simulation strategies with simplified geometry and physics have their place but is this truly enough? What if you could include all the complexities of your geometry and the physics involved in your simulation?

Pages