Library

3038 match your search

Transient simulation of solid stress in a mixer impeller
Transient simulation of solid stress in a mixer impeller
The proposition that “less is more”, first penned by Robert Browning back in 1855, has stood the test of time. It has influenced architecture throughout this century and the last and was keenly assessed in a quote from Frank Lloyd Wright, inspiring the title of this blog today. When we model transient phenomena, it’s easy to generate more data than we can practically work with. We’re driven to it by physics – some processes are inherently unsteady (acoustics, external aerodynamics, in-cylinder combustion, mixing,…). If we can’t efficiently understand and communicate our results, more files, consuming more disk space and resources, is definitely no good. So how do we get to less? With STAR-CCM+ v12.06, our Solution History (.simh) capability comes into play once again, making it possible for you to create effective time history plots quickly and easily from your .simh content without having to take the time and effort to re-run your analyses. And that’s just the beginning...
Transient fluid structure interaction simulation of a mixer impeller
Transient fluid structure interaction simulation of a mixer impeller
Simulation history of solid stresses on a mixer impeller
Simulation history of solid stresses on a mixer impeller
In the past decade, the CFD simulation of combustion processes has advanced beyond all recognition, as the advent of inexpensive super-computing makes use of complex chemistry and large eddy simulation (LES) increasingly affordable. The latest release of Simcenter STAR-CCM+ makes realistic combustion simulation more accessible than ever with the introduction of dynamic mechanism reduction and subgrid spark ignition for LES
Here in the UK, we are not known for large amounts of sunshine but this summer was the greenest ever for energy, largely driven by the huge growth in the number of solar and wind farms. Between May and September 2017, over 50% of power came from low-carbon sources, compared with 35% in 2013. The energy mix for power generation is changing rapidly, driven by the global goals agreed in Paris to significantly reduce greenhouse gases from electricity production. Natural gas power stations play a vital part in this effort, open and combined cycle gas turbines are increasingly being used to smooth out the peaks in power generation, balancing intermittent wind and solar.
三角翼バタフライ風車の構造と流体力のSTAR-CCM+による解析
低コストの小形風力発電機を目指して、過回転抑制機構を備えた風車ロータ直径7mの三角翼バタフライ風車(5枚翼の垂直軸型風車)を現在開発中である。本発表では、この風車の1つのアルミ製三角翼を対象として、STAR-CCM+を用いた構造解析と3次元数値流体力学解析をそれぞれ実施したので、その結果を報告する。また、構造と流体の連成解析も試みており、その状況や可能性について簡単に報告する。
舞台演出用スポットライトの熱対策について
従来、演出用照明器具の光源には、大容量のハロゲン電球が使用されてきた。しかし近年LEDの高効率化と大容量化が進み、COBと呼ばれる高密度に実装されたLED素子を使用することで非常に強い明るさを得られることが出来ている。しかし高密度に実装されたLEDは熱の集中が大きく、LED自身の熱で性能を損なう可能性がある。そのため、LEDに対する熱対策の重要性は高く、中でも熱の振る舞いを解析することは必須と言える。 今回はLEDを使用したスポットライトの熱流体解析を行う。
低コストの小形風力発電機を目指して、過回転抑制機構を備えた風車ロータ直径7mの三角翼バタフライ風車(5枚翼の垂直軸型風車)を現在開発中である。本発表では、この風車の1つのアルミ製三角翼を対象として、STAR-CCM+を用いた構造解析と3次元数値流体力学解析をそれぞれ実施したので、その結果を報告する。また、構造と流体の連成解析も試みており、その状況や可能性について簡単に報告する。

Pages