Library

3038 match your search

Solid handling and processing are widely carried out in process and steel industries. For examples – charging of solid raw materials into a blast furnace; injection of solid coal particles into a blast furnace along with hot gas; conversion of solid coal into solid (porous) coke in a coke-making unit; transport of coal, pneumatic conveying of sintered pellets, etc. Modeling the flow of these solids employing continuum approach has proved to be a big challenge for the researchers. Proper insight into the mechanics that cause the motion of the granular material is still not achieved. Recently,...
The policy framework regulating the emissions of oxides of nitrogen from industrial and utility boilers is in flux. As such, most owners are taking the opportunity to evaluate potential strategies for when, not if, more stringent NOx reduction regulations are put into service. The armada of aging, moderately sized boilers that have been skipped over in the previous wave of Selective Catalytic Reduction (SCR) installations, due to an assumption that they would be eventually replaced with new generation assets, are now in focus as owners are forced to extend the expected lifetimes of these...
In some countries, summer over-heating is a big problem in a building’s energy balance. Ventilated façades are a useful tool when applied to building design, especially in bioclimatic building design. A ventilated façade is a complex, multi-layer structural solution that enables dry installation of the covering elements. The objective of this paper is to quantify of the improvement in the efficiency of the thermal behaviour of buildings when this sort of façade is installed. These improvements are related to the ventilation capacity of the additional structure to the shield mainly for saving...
Computational Fluid Dynamics has been integrated as a key component of missile aerodynamic performance analyses at Lockheed Martin Missiles & Fire Control for many years. Applications are varied, including preliminary aerodynamic databases, identifying component loading, investigating complex flow fields, and assessing safe separation. A discussion of the procedures and tools used is presented, with specific emphasis on STAR-CCM+. Aerodynamic performance predictions from STAR-CCM+ and an in-house code are compared to wind tunnel test data at several Mach numbers for the Joint Common...
A mesh optimization strategy for accurately estimating the drag of a ground vehicle is proposed based on examining the effect of different mesh parameters. The optimized mesh parameters were selected using a Design of Experiments (DoE) method enabling simulations to be carried out in a limited memory environment, and in a timely manner; without compromising the accuracy of results. The study was extended to take into account the effect of model size. A simplified car model at three scales has been investigated and compared with results from the MIRA model wind tunnel. Parameters that lead to...
A detailed theoretical/numerical framework is established to study the mechanical erosion of graphite nozzle materials in solid rocket motors at practical operating conditions. The propellant considered is aluminized AP/HTPB composite propellant. A combined Eulerian-Lagrangian approach is used to treat the multiphase flow inside the motor. The multi-component gas-phase dynamics is modeled using the conservation equations of mass, momentum, and energy in the Eulerian framework. Turbulence closure was achieved using the standard k-epsilon two-equation model. The dispersed phase consisting of...
The present paper covers the work made in order to be able to perform standard deep water IMO manoeuvring simulations based on a combination of computed and measured hydrodynamic input data.Based on a full set of measured PMM data a reduced test matrix was identified and the standard 10-10 and 20-20 zigzag and the 35 turning circle manoeuvres was simulated. Based on the reduced test matrix all the static PMM conditions were computed with the RANS code STAR-CCM+ in order to obtain the hydrodynamic forces and moments. The computed static PMM data was subsequently used to replace the...
Large Eddy Simulation of an incompressible fluid in a straight pipe with a circular cross-section is investigated with a Finite Volume (FV) method based on polyhedral cells, using synthetic turbulence at the inlet. Results of this non-periodic simulation are quite accurate after 2 diameters from the inlet, showing that the structures are self-sustainable. The method is then extended to a flow in a 180˚ U bend pipe with circular cross-section, using an original automatic and boundary-layer-adapting meshing technique. This configuration, or a more convoluted version of it, is often encountered...
Large-eddy simulation (LES) has been performed for an axisymmetric piston-cylinder assembly with and without swirl. For both cases, the LES mean and rms velocity profiles show better agreement with experimental data than profiles obtained using a Reynolds-averaged Navier–Stokes (RANS) approach with a standard k − ε turbulence model. The sum of the resolved and modeled contributions to turbulence kinetic energy (TKE) approaches grid independence for the meshes used in this study. The sensitivity of LES to key numerical and physical model parameters has been investigated. Results are especially...

Pages