Library

2964 match your search

CFD methods and lyophilization: Advancing manufacturing processes to match growing demands
As an effect of globalization, the patent life of newly discovered drugs has decreased considerably, forcing manufacturers to minimize drug development time as well as maximize throughput. To achieve this, existing manufacturing processes need to be upgraded, and new approaches and methodologies developed. Simulation applying CFD and optimization is an ideal tool to investigate such concepts early in the design phase, tying it into the Product Life Cycle Management Process – and thus avoiding costly troubleshooting exercises later. In this webcast, you will learn more on how the integration...
To produce products at the lowest possible cost and high quality while meeting safety requirements, companies in the chemical and mineral processing industries must optimize all elements of their operations to stay competitive. Handling equipment such as pneumatic conveyors, hoppers, chutes and belt conveyors is used for the transport of particles. Processing equipment such as cyclone separators, calciners, dryers and coaters are used for various unit operations. Process engineers need to take into consideration not only the flow of particles but also that of a carrier fluid. The intricate...
This workshop takes a look at different levels of simulation in use today, that guide virtual product design in Li-ion batteries and cooling system management for battery packs. Specialists will highlight state-of-the-art technology, and how they are delivering added value and time savings to engineers.
This workshop takes a look at different levels of simulation in use today, that guide virtual product design in Li-ion batteries and cooling system management for battery packs. Specialists will highlight state-of-the-art technology, and how they are delivering added value and time savings to engineers.
With devices involving the combustion of gas – whether that is a gas turbine combustor, a furnace burner, an industrial process heater or boiler, a burner of a stovetop appliance, or a gas-fired water heater – if your primary objective is to use simulation to “discover better designs, faster” – then I’d say that yes, CFD performed with STAR-CCM+ can be trusted to help you achieve that goal.
시뮬레이션을 통한 고온 공정에서의 운영 우수성 확보
업계의 추세는 에너지 효율을 높이고 환경에 대한 영향을 줄이며 연료 유연성을 높이고 시스템 신뢰성과 처리량을 향상시키는 것입니다. 이러한 업계 추세의 구현을 통해 엔지니어는 비즈니스에 긍정적인 영향을 줄 수 있습니다. 연소 및 반응이 수반되는 고온의 공정은 유리, 제강, 시멘트, 야금, 정제 및 석유/화학 산업에서 흔히 나타납니다. 이러한 목표를 달성하려면 다음과 같은 공정과 장비 설계에서의 혁신이 필요합니다. 가스 및 석탄 버너 유리 및 제강 처리 공정 및 원유 히터 개질기 건조기 및 화로 등 엔지니어들은 이러한 시스템을 설계하기 위한 방법론적 접근법을 사용하기 위해 전산 유체 역학(CFD)과 연소 과정에 대한 반응 운동 시뮬레이션에 점점 더 의존하고 있습니다. 동영상 강의에서는 기술적인 문제 해결 및 혁신을 통한 비즈니스에서의 이득을 얻기 위해 시뮬레이션(CFD 시뮬레이션 및 설계 공간 탐색)을 사용하는 방법에 대한 몇 가지 사례를 살펴 보겠습니다. 우리의 기술 전문가가 이런 모델을 설정하는 과정을 시연할 예정입니다
About four years ago, I was invited to an event near SEATAC airport at a friend’s house on a hot summer day. I remember being surprised by the nearly constant noise from aircraft on approach for landing. I asked the host how he managed to live with the noise, to which he explained that he was working with airport officials to reduce noise levels which should help. Last summer, he invited me over to his home for an event and I was pleasantly surprised by the much-reduced sound levels. It was incredible just how much quieter it was since the last time I was there. This is the case all across the country and, in fact, the world - urban airports are getting quieter, but how?
Using multiphysics simulation to reduce airport noise challenges
Airport noise regulations have tightened in the last decade, making it ever more difficult to operate in urban environments. At the same time, the demand for air travel has been growing. Airport airframers have been searching for ways to reduce the level of perceived noise caused when aircraft land. To that end, innovative companies like ATA Engineering recently demonstrated a prototype aircraft drag management device called an engine air-brake (EAB) in a series of ground tests. The EAB uses a deployable swirl vane mechanism to switch the operation of a turbofan’s exhaust stream from thrust...
This seminar will focus on a variety of engineering simulation topics such as multiphase flows, conjugate heat transfer, secondary flows, cavitation and erosion, and design exploration that are frequently used for improving the design of pumps. We will also examine the latest feature-based case studies to demonstrate the effective use of these functions. Examples related to improving performance in terms of efficiency and reliability, as well as how to reduce the cost of prototyping and experimentation, will be examined.
网络研讨会: 设计能够应对气候挑战的船只——船舶设计的典范转变
海洋产业的诸多企业越来越意识到,应对气候变化需要联合行动,市场格局的竞争愈演愈烈,如要生存下来并持久繁荣昌盛,迫切需要开发新的创新型产品和业务模式。 受油价下跌和全球经济颓势的影响,不论是新起之秀还是老牌企业都一致认为,成败的关键取决于如何适应并从容应对这些异动。 本网络研讨会将介绍如何以新颖详尽的方法利用仿真帮助海洋产业企业实现创新目标,从而达成企业目标。利用仿真技术自动探索设计空间不仅可帮助企业提高生产力,而且还可帮助工程设计人员聚焦创新设计,从而继续创造出更好的船舶性能以及凸显其竞争优势。 我们将通过采用基于仿真技术的方法来优化商业船只的初始设计以演示这一转变设计优化将考虑到不同的航行条件以及推进器设计。 这种方法将展示现实世界基于仿真技术的初始设计,还将演示如何从设计流程的最初阶段应用宝贵的研究。

Pages