Library

3038 match your search

Using STAR-CCM+ for Catalyst Utilization Analysis
Due to increasingly stringent emissions requirements, 3D CFD has been used extensively at Ford for the development of exhaust and after treatment systems, for example to assess the catalyst utilization. In order to maintain the quality of the analysis which could be carried out by CAE teams inside and outside the company, we have developed a unique CAE procedure which standardizes the ways to perform the analysis, post-processing and presentation. This presentation describes how we upgraded this procedure from STAR-CD to STAR-CCM+ standard.
Emergency Ventilation System Modeling
Architects and engineers are continually pushing the limits of design through the use of novel building shapes and mixed mode ventilation systems. Analysis techniques must be sufficiently sophisticated to follow suit, especially with respect to the life safety aspects of the design. The mixed mode emergency ventilation system described in this work and proposed for a semi-enclosed bus terminal is a typical example. The terminal connects to a pedestrian mall and has a unique scalloped façade. STAR-CCM+ was used to aid in the design of the emergency ventilation system consisting of sprinklers...
DARS SRM as Combustion Model for Engine Concept Development
New combustion concepts like PPC and RCCI have demonstrated very high indicated efficiencies together with a potential for low engine out emissions. But the implementation of those combustion concepts in engine concepts remains a challenge. A number of issues like boosting, load range, EGR control and transients have to be addressed. Integration of different technologies into an engine concept is done with gas exchange simulations. But how is the combustion in the gas exchange simulations modeled when new combustion concepts are utilized? Iterating with 1-cylinder testing and 3D combustion...
Application of Direct Quadrature Method of Moments in Multiphase Flows using STAR-CCM+
Commercial fluidization technologies can benefit from a deeper understanding of the interplay between the dynamics of the fluids and solids in these multiphase processes. Dispersed-phase and particulate systems, such as precipitation, crystallization, particle formation in aerosols and fluidization, can be modeled using the Population Balance Equation (PBE) approach to describe different particle properties. In our research, we have implemented this PBE approach into our High Performance Computing (HPC) STAR-CCM+ simulations. In particular, we are using the Direct Quadrature Method of Moments...
Improving Layer Control in Multi-Layered Polyester Films using Computational Fluid Dynamics (CFD)
Polyester based Multi-Layered Films (MLFs) form a major part of DuPont Teijin Films' (DTF) product portfolio. Such MLFs are formed when different polymer melt layers come together in a process known as coextrusion. The main coextrusion geometries used at DTF are: • an injector block linked to a die and • a multi-manifold die. As the thickness and melt flow properties of the layers become more differentiated, it becomes more difficult to control individual layer width and thickness of an MLF. CD-adapco’s STAR-CCM+ is used to improve the layer control of current MLFs, reducing the potential...
Conjugate Heat Transfer Analysis of a High Loaded Convection Cooled Turbine Vane with STAR-CCM+
The importance of coupled simulations of aerodynamics and heat transfer in the development of stationary gas turbines and aero engines is growing steadily in order to minimize development costs and effort. Conjugate heat transfer calculations can reduce those efforts and cost significantly, e.g. by reducing the quantity of experimental tests. As a result, the quality of numerical results becomes an important issue. In addition, due to more and more complex models, the set-up and validation of the numerical calculations is also of high importance. This presentation will show the set-up and...
Duct Pulsation Problem Captured & Solved using STAR-CCM+
A recently installed Victory Energy boiler is supplied with fresh air through custom ductwork supplied by a third party. This custom ductwork was subject to severe space limitations. During the initial startup, vibrations occurred in the ductwork between the fan and the burner windbox. As the load reached 50%, the frequency and strength of these vibrations increased to the point where they threatened the structural integrity of the ductwork. Even though they had not supplied the ductwork, Victory Energy hired BMA to pinpoint and address this problem. Steady state CFD simulations of the...
Thermal Simulation of LED-Powered Luminaire with Coupled Electrical Circuit Analysis
LED manufacturers sort LEDs into 'bins' based on the forward voltage to give their customers the most consistent light color possible. Manufacturing tolerances can cause a range of colors even in the same batch of LEDs, so this binning process gives their customers higher consistency in the color produced. Despite the tight grouping of forward voltages in these bins, inherent LED characteristics can still result in non-homogeneous current draw, luminous flux, heat dissipation and junction temperature. This highly interconnected process was investigated using STAR-CCM+ and SPICE to simulate...
Solar Air Heater Wizard: Automating CFD
Enerconcept Technologies designs, manufactures and installs solar air heating systems. Their wall-mounted solar air heater system is modular and its configuration is customized for each building. Enerconcept had a need to quickly calculate the expected efficiency of each particular configuration and optimize design parameters like inlet/outlet position, wall thickness, etc. Lx R&D proposed to program a wizard that Enerconcept designers could use to easily run CFD analysis with STAR-CCM+ on a particular wall configuration. Relevant information like wall size and sun orientation is entered...
Using STAR-CCM+ for Wind Dispersion Studies
Various regulatory agencies such as the US EPA, OSHA, state and local code enforceme0nt agencies often require environmental impact studies when certain commercial buildings are renovated or newly constructed. Usually, these buildings are laboratories, special environments for chemical or biological agents or manufacturing plants that must discharge chemical effluents into the atmosphere. Other conditions also mandate studies of environmental influence such as large boiler exhaust, emergency power generation, or the effects of diesel trucks idling at critical areas around buildings. The CAES...

Pages