Library

2996 match your search

The Italian challenge at the Little America’s Cup 2013: Design and analysis method for the C Class prototypes
The Italian challenge at the Little America’s Cup 2013: Design and analysis method for the C Class prototypes
Welcome & Cervélo Keynote
Welcome & Cervélo Keynote
Experimental Validation of STAR-CCM+ for Liquid Container Slosh Dynamics
The NASA Launch Services Program has funded several propellant slosh related projects over the years with the goal of obtaining experimental data to anchor CFD predictions. STAR-CCM+ is used to create a CFD model of water sloshing in an 8” diameter spherical tank. The predictions from this CFD slosh model are compared to experimental data to validate the results. The data compared include slosh natural frequency, damping rate and free surface topology. These important validations allow us to increase our confidence in STAR-CCM+ for use on NASA missions.
An overview of battery simulation
An introduction to batteries is provided, including an overview of the commercial value of batteries sold by chemistry. Opportunities for battery simulation in various markets (automotive, consumer, industrial, etc.) are presented, along with examples of the STAR-CCM+ BSM module and Battery Design Studio.
CFD Study of an Industrial Heater
A CFD study using STAR-CCM+ 7.04 is performed to simulate an industrial heater with burners firing refinery gas fuel. The heater has been reported with short run length due to coking inside the process tubes. Heater, burners and combustion air duct are included in the modeled geometry. Turbulence, combustion and radiation models are activated to simulate the environment inside the heater. System analysis is performed such as combustion flame pattern, temperature and velocity fields, heat flux and temperature distribution at various locations etc. Non-uniform heat flux distribution on process...
Optimate Evaluation: Design Optimization of a Generic Glider
One of the difficulties of optimization of any design using CFD is the sheer number of runs required using traditional methods. This presentation details the use of Optimate for the optimization of a generic glider. This case was designed to stress the SHERPA algorithm with a realistically complex set of design criteria to optimize an aerodynamic vehicle, including stability requirements and trimmed L/D performance requirements.
V3 in Fire & Smoke Analysis
As capabilities and features in STAR-CCM+ continuously become more numerous and sophisticated, there is an increasing demand in Verification, Validation and Visualisation. Especially in general engineering and building services, where customers do not have a distinct CFD background, the simulations have to bear more critical assessments because of targeting a more sceptical audience. Thus, it is extremely essential to validate simulation against experiment, empirical approach and literature most intelligible to a wide range of customers and show the results in a vivid and realistic way. Still...
Using STAR-CCM+ for Catalyst Utilization Analysis
Due to increasingly stringent emissions requirements, 3D CFD has been used extensively at Ford for the development of exhaust and after treatment systems, for example to assess the catalyst utilization. In order to maintain the quality of the analysis which could be carried out by CAE teams inside and outside the company, we have developed a unique CAE procedure which standardizes the ways to perform the analysis, post-processing and presentation. This presentation describes how we upgraded this procedure from STAR-CD to STAR-CCM+ standard.
Emergency Ventilation System Modeling
Architects and engineers are continually pushing the limits of design through the use of novel building shapes and mixed mode ventilation systems. Analysis techniques must be sufficiently sophisticated to follow suit, especially with respect to the life safety aspects of the design. The mixed mode emergency ventilation system described in this work and proposed for a semi-enclosed bus terminal is a typical example. The terminal connects to a pedestrian mall and has a unique scalloped façade. STAR-CCM+ was used to aid in the design of the emergency ventilation system consisting of sprinklers...

Pages