Library

2927 match your search

Formula 1 Fuel Tank sloshing
Formula 1 Fuel Tank sloshing
Formula 1 Fuel Tank Sloshing
Formula 1 fuel tank sloshing
The new automatic time stepping in STAR-CCM+® v11.04 automatically adjusts the timestep size of simulations dynamically. This helps to reduce time to achieve solutions for transient runs by avoiding the use of unduly small timesteps.
 Designing Under-Body Components Using Leading Wading Simulation Methods
Vehicle water wading capabilities refer to vehicle functional part integrity (engine under-tray, bumper cover, plastic sill cover, etc.) when traveling through water. Wade testing involves vehicles being driven through different depths of water at various speeds. The test is repeated and under-body functional parts are inspected afterwards for damage/leakage. The lack of computer aided engineering (CAE) capability for wading equates to late detection of failure modes, which inevitably leads to expensive design change. Critically, this can potentially affect program timing. As a result, it is...
2016年6月13日-15日,由CD-adapco China举办的“STAR 2016中国用户大会”在杭州隆重召开。
Design Exploration with CFD for Better Dry Low NOx Hydrogen Gas Turbine Combustors
Safely combusting hydrogen (H 2 ) in gas turbines, while still providing sufficient energy density, could help meet ever-increasing energy demands by making use of an economically attractive fuel supply. For instance, some of the electricity intermittently produced by some renewable energy sources such as wind and solar could be used to produce hydrogen, which is then used to power gas turbines (GT) to help meet peak energy demands, especially at times when the wind isn’t blowing and the sun isn’t shining. By viewing this webcast, you will hear from guest presenter Anis Haj Ayed from B&B-...
Custom Sim Trees in STAR-CCM+ v11.04 are a fundamentally new way to work with the sim tree, allowing users to create smaller node trees in a separate window for less scrolling and easier navigation overall.
STAR-CCM+ v11.04, now part of the Siemens Simcenter™ Portfolio, is aimed at empowering engineers across industries to make critical design decisions quickly and with confidence through new modeling capabilities, improved simulation workflows and reductions in overall time-to-solution.
The automotive industry is one of the most thriving and competitive industries. There are many challenges OEM’s face when produce new vehicle today. Those challenges include meeting stricter emission regulations to need for improved customer satisfaction. This drives the need to bring vehicles faster to market while meeting new challenging designs. OEM’s are turning to simulation to help drive design to produce innovative vehicles while reducing costs. One challenge of working with the digital prototype is determine heat protection for critical components in the engine compartment. To solve...
STAR-CCM+ is now part of the new Simcenter™ Porfolio for predictive engineering analytics. Simcenter combines simulation and physical testing with design exploration and data analytics to help customers develop digital twins that accurately predict product performance.

Pages