Library

2922 match your search

State of the Art CFD for Military Ground Vehicles
Engineering simulation using computational fluid dynamics (CFD) has grown rapidly in recent years due to significant advances in geometry preparation, meshing, physics modeling and numerics. With demanding schedules, shrinking resources and a competitive market, engineers and scientists need to obtain accurate results as quickly and efficiently as possible. This webcast offers and demonstrates capabilities for solving modern design and analysis challenges relevant to military ground vehicles using engineering simulation. CFD Specialists highlight the efficiencies of using an all-inclusive pre...
Last week we announced the release of STAR-CCM+ v8.04, the second of our three v8 series for 2013. I can see from the download logs of the Steve Portal that many of you downloaded the new version within the first few minutes. I hope you are enjoying all the new features and enhancements. While I could talk at length about these new bells and whistles , I'd prefer to explain the rationale behind STAR-CCM+ v8.04, and explore the philosophy of our development strategy. One of the consequences in maintaining our aggressive release cycle is that it’s easy to become distracted by the list of...
Motorcycle Dirt and Water Management
STAR-CCM+ v8.04 simulation of a motorcycle travelling through a film of surface water.
Airbus on Advanced Modeling and Simulation
During this one hour event Martin Schmid from Airbus discusses how shorter development cycles are the key for competitive advantage in the aircraft industry. He will investigate how achieving this competitive advantage requires the analysis of system performance and reliability at an early stage to reduce the risk of late equipment changes with impact on the schedule. Specifically Martin addresses how quality computational fluid dynamics (CFD) is required with validated models to meet the criteria. Examples and demonstrations in this event focus on environmental control systems, and how...
Modeling Internal Combustion Engine In-Cylinder Processes
Addressing IC Engine performance using the latest modeling techniques. There are many tough challenges facing manufacturers of IC Engines to reconcile legislative and market demands and up-front simulation has now become integrated into the product design process in most vehicle and engine companies throughout the world. This webcast highlights some of the latest developments in numerical simulation of in-cylinder flow, fuel spray mixing and combustion that are becoming available to engine analysts. Examples illustrate new methods for accurately simulating fuel injection and sprays and how...
Dirty or Not, Taking CAD Directly to CFD Simulation…The Easy Way!
Dealing with the consequences of imperfect CAD has long been the biggest bottleneck in CFD. This key fact was, until recently, the single largest obstacle in getting flow-simulation to have a real positive impact on product development. For a typical case, producing a meshing quality triangulated surface, along with the required high quality computational meshes from complex or dirty CAD, could take days or even weeks. Ultimately, up to 50% of the engineering budget can be consumed. It is not just automated surface clean-up; this on-demand webinar recording demonstrates the latest surface...
We've all been mesmerized for years by that thing of beauty rising out of the water majestically in that James Bond movie... If you're thinking Ursula Andress or Halle Berry or Daniel Craig, think again. I'm an Engineer and to me, the submarining Lotus Espirit from The Spy who Loved Me is my equivalence of a teenager's infatuation with water entry of matinee idols. In my fantasy world, my car would run on road, swim in water, fly in air and even brew me a nice, cold beer while I watch football. The Lotus Espirit ticked off two of those boxes quite handsomely. When I was tasked with showing...
The Need for Speed – High Performance Sports Turn to Digital Simulation
This event features examples from the NASCAR company, Michael Waltrip Racing and Cervélo Bicycles, a competitive tour and Olympic cycling company. Get a sneak preview from Waltrip.
Electronics Best Practices Part 3: Thermal Radiation
Radiation is one of the three fundamental modes of heat transfer, yet it is often ignored in electronics cooling simulations. One of the reasons it is often ignored is that the core physics are not fully understood. Additionally, the impact of radiation on the predicted temperatures is underestimated, especially in natural convection simulations. The core physics of radiation as it applies to electronics cooling is discussed in this online seminar, including the visible and infrared radiation spectrum, relevant material properties, solar radiation, and internal radiation. CFD specialists...
Unsteady simulation of a spinning shuttle cock with Transition Modeling
Animation from an unsteady simulation of a shuttle cock with Gamma-Re-Theta transition modeling showing pressure contours on the shuttle cock and flow streamlines.

Pages