Library

2923 match your search

CD-adapco는 최근 서울에서 STAR Korean Conference 2013을 개최하였습니다. 2013년 12월 18일, 서울 CD-adapco 는 12월 5일과 6일 양일간 서울 JW 메리어트 호텔에서 2013년도 STAR Korean Conference를 개최하였습니다. 이는 CD-adapco Seoul Office에서 실시하는 가장 큰 연중행사로 자동차/전기/전자/조선/항공/터보기계/국방/에너지/원자력/화학/건축환경/배터리 등 다양한 분야의 전문가들이 모여 최신 해석 기술과 현업에서의 연구 경험을 함께 나누는 국내 최대 규모의 CAE 컨퍼런스입니다. 양일간 행사에서 70여편의 논문들이 발표되었으며, 난류 및 열 전달 이론 교육을 비롯하여 직접 실습을 통해 배울 수 있는 CAD to Mesh, Meshing Best Practice, 그리고 Design Exploration 교육이 개설되어 많은 호응을 얻었습니다. STAR-CCM+의 개발을 총괄하는 Jean-Claude Ercolanelli가 STAR-CCM+에 새롭게 추가된 기능을 비롯하여 앞으로의 개발 방향에 대해 발표하였으며, 이 외에도 CD-adapco내 전문가들이 다양한 산업에서...
Heat Sink Optimization Using Simulation of the Entire Operating Range
Heat sinks have long been a key component of the thermal management strategy of electronic components and they will continue to be used for the foreseeable future. The goal in any heat sink selection process is providing adequate heat transfer at a minimum cost in the available space envelope and often minimizing the mass of the heat sink. Achieving this goal is valuable for both the heat sink manufacturer and the system designer, but the large number of variables that need to be investigated can make it difficult to accomplish. Physical testing of the range of heat sink variations takes both...
A youtube video demonstrating co-simulation work done with cd-adapco's STAR-OLGA and STAR-CCM+ software, showing advanced meshing techniques and multiphase fluid flow.
For more than two decades Access has been successfully following the strategy to qualify its science addressing research topics of technological relevance. A creative environment and a state of the art infrastructure support an international and interdisciplinary team. Access teams up with a number of selected partners that broaden and enhance its knowledge and capabilities.
3D CAD to Meshing – Why This Is Critical For Production Level CAE Today
To achieve high levels of certainty with CFD it is essential to generate high quality meshes starting from CAD data. High productivity workflows and optimization necessitate that meshing must be easily automated and robust. This webcast covers distinct capabilities for moving your CAD geometries through to meshing. Presenters show a unique bi-directional communication between STAR-CCM+ and all of the major CAD packages. This process demonstrates how to simplify and streamline existing CAE protocols. In addition, using expanded 3D CAD capabilities, presenters illustrate the options within STAR...
CD-adapco recently hosted an engineering simulation conference for the Oil and Gas and Chemical industries in Houston, TX. New York and London. December 5, 2013 CD-adapco, the largest privately held CFD focused provider of Computer Aided Engineering software, recently held a conference focused on the application of Computational fluid dynamics for the Chemical Processing and Oil and Gas industries featuring presentations from The Dow Chemical Company, Shell, Norton Straw, Eastman Chemical, MSI Kenny, University of Houston, PNNL, and ExxonMobil. The keynote address at this Houston-based...
External air cooling of an induction machine: The machine interior is totally sealed to prevent dust from entering through very fine air gaps. The external fan is rotating, blowing air outside the machine.
Temperature distribution analysis of an ASCS battery module of 84 cells: 42 cells are connected in series, and each row is connected in parallel. The liquid-cooled plates are lateraly postionned on each side of those rows (Model courtesy of ASCS, Stuttgart and Behr).
Meeting Future Emission Standards with Advanced Engine Simulation
The need for reductions on emissions has never been greater; it is an essential priority to decrease rising air pollution. In addition to emission reduction, legislation is placing the emphasis on engine manufacturers to reduce fuel consumption. Reducing emissions and fuel consumption are often conflicting requirements, so engineers need to work at finding an optimal design. This webcast provides clear and comprehensive strategies for using simulation, improving engine design and therefore lowering overall emissions and fuel consumption. Presenters demonstrate setting up complete processes...
Simulating Systems This edition of Dynamics illustrates how numerical simulation combined with process automation allows engineers to explore the design of entire systems. More than ever, the success stories featured in this edition demonstrate how STAR-CCM+’s extending capabilities are being applied to an ever wider range of applications, including Aerospace, Ground Transportation, Marine, Oil & Gas, Energy, Building Services, Turbomachinery, Chemical Processing and Life Sciences.

Pages