Library

2964 match your search

If you pack too much matter into a small space, you are likely to get some undesirable consequences as anyone vacationing with small kids will be all too aware. If you have to sit on your suitcase to get it closed, you are likely to be greeted by the sight of your holiday clothes circling on the carousel at your destination. Similar consequences befall the engineer simulating two-way coupled fluid-particle systems when they overload cells in the CFD mesh with too much DEM matter. I refer, of course, to the previous requirement that a DEM particle must be smaller than the flow cell it occupies for two-way coupled simulations. This limitation is due to the way the effects of the DEM particle are applied purely to the flow cell in which the particle centroid lies, and not to adjacent cells that are also overlapped by the particle. When DEM particles are larger than the cell, this results in large sources of momentum and energy being applied to individual cells causing instability and divergence. However, it is not just stability that can be compromised, but also accuracy, with the void fraction of the particle not being fully accounted for if the volume of the cell is smaller than the particle. In practice, this rendered some applications impossible to simulate as geometrical features forced the mesh size to be smaller than particles. The recent release of STAR-CCM+® v11.06 changes all that with DEM source smoothing…
Designing ships for future challenges – a paradigm shift in vessel design
To many companies within the marine industry, it is becoming clear that the combined effect of tackling climate change and the increasingly competitive market landscape requires new and innovative products and business models to be delivered at an ever-increasing pace if they are to survive and secure long-term prosperity. Amplified by the downturn in oil prices and the global economy, companies – both new and old – find success or failure based on how they adapt and respond to these circumstances. This webinar will demonstrate how using simulation in new and deliberate ways is helping...
Look around your desk, within reach of you right now. How many things do you see that have a circuit board, a couple of chips and maybe an LED or two in them? I count 12, and that’s just within reach. When you think about the electrification of our world, smaller, more powerful and newest are the three words that describe the value of a piece of electronics. So let’s look at these two statements through the eyes of a typical thermal analyst: “I have to build and analyze, smaller, hotter and faster to stay competitive.” That is precisely the reason we have spent the last few years developing the Electronics Cooling Toolset within STAR-CCM+® software. We recognized that designers in the electronics market need tools to setup, run and analyze their products in STAR-CCM+ but with fewer clicks, more interactivity, and a much more focused interface. This is a tool available to every user, aptly named the Electronic Cooling Toolset, or E-cool for short.
Advancements for in-cylinder analysis and design exploration
STAR-CD ® /es-ice/DARS is a market-leading toolset for in-cylinder CFD simulations that offers the most advanced physical models for combustion and emissions formation. Furthermore, combining such a toolset with design space exploration enables the discovery of more innovative designs to help maximize fuel economy and performance while minimizing the formation of harmful pollutants. View this On-Demand Webinar to get up to speed on the latest developments for the Siemens PLM Software in-cylinder solution and learn how to get better combustion system designs, faster. Topics covered will...
Imagine finally picking up your new Tesla after months of waiting (popular cars have waiting lists). While counting down the days, you daydream about driving that beauty on the freeways and cruising downtown as the commoners turn their heads to catch a glimpse. The last thing you are going to worry about is if the battery is defective or even ineffective. Yet while often overlooked, the battery is arguably the most important part of the vehicle. But don’t worry; chances are that well before you placed your order, computer-aided engineering (CAE) was used to ensure that the battery of your amazing new car will let you feel like Batman and not a Joker.
From overheating phones to underperforming data centers, thermal malfunction of electronics devices is not just a nuisance but a performance and safety risk. It is no secret then that thermal reliability is at the forefront of an electronics engineer’s design concerns. Demand for high power density devices in smaller packaging requires innovative cooling strategies. Traditional simulation strategies with simplified geometry and physics have their place but is this truly enough? What if you could include all the complexities of your geometry and the physics involved in your simulation?
STAR-CCM+ v11.06 새로운 기능 소개
STAR-CCM+® v11.06이 출시되어, 이번 버전에 포함되는 새로운 기능에 대하여 알려드리고자 합니다. 이번 버전에는 전자 장비 냉각 해석 모듈(E-Cool)이 포함되어 있습니다. E-Cool은 보드와 시스템 레벨 전자 장비의 열 성능 해석을 위해 전자 부품들을 쉽게 만들고 조작할 수 있게 해 줍니다. 팬, 방열판, 칩, 보드와 같은 부품들을 산업 표준인 IDF 형태 파일로 불러오거나 STAR-CCM+에서 만들 수 있습니다. 새로운 E-Cool 기능과 함께, STAR-CCM+ v11.06은 사용자들에게 기술, 사용자 경험 및 생산성에서 상당한 이점을 제공합니다. 우리의 주요 목표는 시뮬레이션 결과에 대한 확신을 높일 뿐만 아니라, 중요한 결정을 신속히 할 수 있는 엔지니어링 시뮬레이션 도구를 제공하는 것입니다. 이번 영상에서 소개드릴 주요 기능은 다음과 같습니다. 노즐과 오리피스를 통한 다상 유동, 기포 유동 또는 반 중력 유동과 같은 응용 분야에서 선택적 다중 크기 그룹 균형 ( A-MUSIG) 모델은 사용자들이 다양한 크기 집단을 갖는 분산된 형태의 기포, 액적 또는 입자들을 정확하게 모델링 할 수 있게 합니다. 여과, 유동층 또는 바이오매스...
Mallards, Wigeons, Teals, all are types of ducks, all are decoys that my dad would carve. Sitting in the garage, chisel and rasp in hand, he would spend hours and hours slaving over these delicate models. Each feather required a steady hand and intense concentration, but no matter the skill of the sculptor a hand will slip or a dull instrument will splinter the wood, or a rambunctious child will think they’re helping. So this means for every beautiful bird produced there are at least 10 in various states of duck resemblance in the scrap bin. The final successful carving was really the time...
I once bought a step counter, with a separate heart rate monitor, and it provided lots of interesting information but I never used it. Despite my investment in the technology, it was simply too messy to use all the different devices in addition to my phone.The value of the additional information about my health was probably enough to motivate me, but the disparate technologies prevented me from using them. Today there are step counters and GPS in our phones, and heart rate monitors in our smart watches. With a simple app download you have everything you need, all through devices you already use and bring with you everywhere. By consolidating these technologies into a single device it is now practical to access the information on my health that they provide.

Pages