Library

2922 match your search

Cool is a hard thing to define. It’s completely subjective. But you know it when you see it. There are a lot of ways to present CAE/CFD data. Plots and tables are arguably what we make most of our decisions on. But, “Excel sheets… aren’t everyone’s friend” . Scenes then… you can put a lot of things into your scenes; results on the surfaces of the thing you’re simulating, streamlines that go in and around the thing you’re simulating… These visual abstractions are a deeply ingrained part of our engineering culture. But not everyone has a casual familiarity with this language. People with diverse levels of expertise have to make sense of these abstractions. And those who don’t, or no longer, speak the language daily and who typically have the least amount of time to assemble conclusions, also carry the heaviest decision-making obligations. Maybe some of you are getting ahead of me here, recalling the phrase “Color For Directors,” a phrase I personally find to be demeaning to directors and dismissive of what we do. Cool pictures? Sure, but cool isn’t cool if it isn’t right. I submit that we have an ethical obligation to maintain the fidelity of our data , and taking it a step further, we rely on good fundamental data to make decisions. Now, data alone can’t capture an idea . Effective visualizations (cool is implied here) can capture ideas, quickly and easily, inviting curiosity and engaging broader audiences. In STAR-CCM+® v12.02, you can create photorealistic images and animations, reducing the gap between the time needed for you to communicate your messages and the time needed for others to understand practical implications, quickly placing your information into their own knowledge frameworks.
Using aerodynamics simulation to optimize for pending WLTP requirements
With the shift to improved procedures for fuel consumption and CO2 emissions, a new Worldwide Harmonized Light Vehicle Test Procedure (WLTP) has been developed by the United Nations. The aim of WLTP is to more accurately reflect real-world driving and harmonize emissions testing across the globe. The new testing procedure will begin in 2017 and roll through 2018 in different stages. One key impact of the WLTP is the calculation of fuel consumption/emissions will not just focus on vehicle, engine and transmissions. Engineers will now need to include any special equipment and the weight changes...
We all have seen electric cars on the street. They look very futuristic and demand a second glance from passers-by. And the convenience… you can drive them in the car pool lane, park and even charge it for free in some places. Great! Their price tag is still an impediment to their large adoption by consumers, though, even if incentives exist in many countries. Another reason for their slow expansion is the rather low drive range these vehicles offer. The longest range available on the market is 300 km (a little over 186 miles) in real driving conditions. Although this would be sufficient for the usual daily commute from home to office, people have the feeling this is not enough for the few times a year they’ve got to drive 500 km (over 310 miles), like to go celebrate Grandma’s 90th birthday. Well, we don’t call that selfishness - although we think you should visit Grandma more often - we call this range anxiety, or the fear of being short of gas (or electricity in our case). So that’s 300 km you can do before you have got to spend several hours at the charging station to continue on your journey and be on time for Grandma’s cake. You’d better order a three-course meal, with a long coffee, buy some newspapers and hoover the car to occupy your time while the car is charging. Fortunately, there is a solution to reduce your entertainment bill at the service; it is Fast Charging. If we could charge our EV to full capacity in the same time as we fill our gasoline tanks, range anxiety would not be such a problem. In this blog, we want to explore the complex problem of fast charging with Battery Design StudioTM, understand its implications and see whether there is anything that can be done to remedy this problem.
Automated solution of the inverse problem in electronics cooling
The majority of engineering simulations involve a known geometry, prescribed conditions and computation of the predicted results. However, the design question is often posed as the inverse: I have a desired result and need to know what conditions or what geometry will produce that result. For an electronics cooling situation, the inverse problem description might be that you have a targeted maximum temperature for the components and you need to determine what geometry will produce this for a given set of conditions, or alternatively, what are the maximum heat dissipations allowed for a given...
最適化ツールの導入をご検討のお客様を対象に、設計探査作業(最適化、 実験計画法、応答曲面等)の一連の流れを例題を通じてご体験いただけます。
STAR-CCM+の導入をご検討のお客様を対象に、モデリングから 計算実行・結果処理までの一連の流れを実際に操作体験いただけます。
STAR-CCM+の導入をご検討のお客様を対象に、モデリングから 計算実行・結果処理までの一連の流れを実際に操作体験いただけます。
STAR-CCM+の導入をご検討のお客様を対象に、モデリングから 計算実行・結果処理までの一連の流れを実際に操作体験いただけます。
最適化ツールの導入をご検討のお客様を対象に、設計探査作業(最適化、 実験計画法、応答曲面等)の一連の流れを例題を通じてご体験いただけます。

Pages