Technical Library

Some articles have copyright restrictions,
in order to download these you will be redirected to the copyright holder's website.

 
Name降順で並び替える Author(s) Date
Accurate & Efficient Turbomachinery Simulation Chad Custer
Numerical Simulation of High Lift Trap Wing using STAR-CCM+ Prashanth Shankara and Deryl Snyder 6月 25, 2012
0D/1D after-treatment modeling with DARS Fabian Mauss
1-D/3-D Co-Simulation of Environmental Control System for Aircraft Klaus Wolf
1-D/3-D Co-Simulation of Environmental Control System for Aircraft Klaus Wolf
1D-3D連成によるエンジンコンパートメント熱収支解析手法の提案 緒方 洋介
3-D Numerical Modeling of Unsteady Heat Transfer in a Rectangular Duct K. Isa, I. Ekmekci, H. Guven, N. Sozbir 8月 2, 2009
3D CAD Kim Eung Ju
3D Conjugate Heat Transfer Analysis of the Next Generation: Inner Reflector Plug for the Spallation Neutron Source Ashraf Abdou
3D Micro-Structural Electrochemistry model 8月 1, 2013
3D Numerical Modeling of the capacity for a partially pressurized Spillway Samuel Vingerhagen, Nils Reidar B. Olsen 2月 1, 2012
3D-CAD Kim Eung Ju
3D-Electrochemistry: Designing and resolving the microstructure of an electrode Gaëtan Damblanc
40-Ton Articulated Truck Cooling System Modelling Using STAR-CCM+ Gary Yu, Martin Timmins, Mario Ciaffarafa
A CFD study of heating steel bar end face to allow machinability Eike Runschke, Zeljko Cancarevic, Axel Stüber, Henning Schliephake
A CFD Study of Particle-Laden Flow of a Tundish Water-Model Eike Runschke, Zeljko Cancarevic, Henning Schliephake
A CFD Study of Wind Turbine Aerodynamics Chris Kaminsky, Austin Filush, Paul Kasprzak, Wael Mokhtar 1月 1, 2012
A Co-Simulation Approach to Modeling the Solenoid Valve Multiphysics Sharat Prasad, Kaushik Das, Krishna Gundu
A Combined Electromagnetic and Thermal Approach to the Design of Electrical Machines D. G. Dorrell, M. I. McGlip, M. I. McGlip
A Comparison of Modeled and Measured 3-D In-Cylinder Charge Motion Throughout the Displacement of a Four-Valve SI Engine Hans G. Hascher, Harold J. Schock, Oshin Avanessian, James Novak 1月 1, 2003
A Comparison of RANS-Based Turbulence Modeling for Flow over a Wall-Mounted Square Cylinder P. L. Davis, A. T. Rinehimer, and M.Uddin 4月 4, 2012
A comprehensive solution for efficient combustion simulation with detailed chemistry Fabian Mauss
A Computational Approach for Optimizing the First Flyer Using STAR-CCM+ Abdul H. Aziz 7月 31, 2013
A Computational Fluid Dynamics Study of Air Mixing in a Naturally Ventilated Livestock Building with Different Porous Eave Opening Conditions T. Norton, J. Grant, R. Fallon, D.W. Sun 6月 1, 2010
A Computational Study of Icing Effects on the Performance of S-Duct Inlets Wonjin Jin, Ray Taghavi 7月 21, 2008
A coupled CFD-population balance approach for nanoparticle synthesis in turbulent reacting flows Ethro Akroyd, Alastair J. Smith, Raphael Shirley, Laurence R. McGlashan, Markus Kraft 2月 9, 2007
A fast and easy optimization tool for electric rotating machine design Luca Gregorio Frigoli
A First Contact with STAR-CCM+: Comparing Analytical & Finite Volume solutions with STAR-CCM+ Simulations Michael Heyer
A Functional Method for the Optimization of Offshore Platform Orientation Utilizing Computational Fluid Dynamics Gerard Reynolds
A means of avoiding sulfur recovery reaction furnace fired tube boiler failures Mike Porter, Dennis Martens, Sean McGuffie, John Wheeler
A method to dynamically estimate the diffusion boundary layer from local velocity conditions in laminar flows Fabien Jousse, Thibauld Jongen, Wim Agterof 1月 4, 2005
A Multi-Disciplinary Approach for Design Improvement of an Air-Cooled Two-Wheeler Engine Cylinder Head Om Singh, T. Sreenivasulu, M. Kannan, K. Nagaraja 9月 28, 2010
A Multiscale Model of the Neonatal Circulatory System Following Hybrid Norwood Palliation Andres Ceballos
A Multiscale Model of the Neonatal Circulatory System Following Hybrid Norwood Palliation A. Ceballos, A. J. Kassab, E. A. Divo, R. D. Osorio, R. Argueta-Morales, W. M. DeCampli 3月 31, 2011
A New Decoupled CFD and FEM Methodology for the Fatigue Strength Assessment of an Engine Head S. Fontanesi, D. Carpentiero, S. Malaguti, M. Giacopini, S. Margini, L. Armone 5月 14, 2008
A new meshing methodology for faster simulation of a Body-In-White dipping process Madhusudhan Devanathan
A NEW VIRTUAL COILING METHOD AND ITS USE IN EVALUATION OF COMBINING COILING AND FLOW-DIVERSION TREATMENT IN A PATIENT-SPECIFIC ANEURYSM Robert Damiano, Jianping Xiang, Elad Levy, Hui Meng 8月 17, 2014
A Numerical Analysis on Air-cooling Performance of Passenger Cars 4月 12, 2010
A Numerical Approach to Thermal Management of Dynamic Driving Cycles Mario Disch (Daimler AG), Thomas Walker (CD-adapco)
A numerical investigation of thermal conditions and deformations of the Astronomical Roentgen Telescope Alexander A. Ryabov, Victor D. Spirin, S.Y. Gulakov, S.G. Garanin, S.V. Grigorovich, M.N. Pavlinskyi, N.P. Semena
A numerical method of modeling oil jet piston cooling
A PEM Fuel Cell Distributed Parameters Model Aiming at Studying the Production of Liquid Water Within the Cell During its Normal Operation: Model Description, Implementation and Validation O. Suria, E. Testa, P. Peraudo, P. Maggiore 4月 12, 2011
A PRAGMATIC APPROACH TO CFD MODELLING OF SEPARATION PROCESSES Kristian Etienne TRÆTLI-EINARSRUD, Balram PANJWANI, Vincent PAUCHARD 6月 17, 2014
A robust and efficient finite volume scheme for the discretization of diffusive flux on extremely skewed meshes in complex geometries Philippe Traoré, Christophe Louste, Yves Marcel Ahipo , Paul Sabatier Toulouse 8月 1, 2009
A Shared Vision: Shaping the Future of Biomedical Device Design & Diagnostics through Modeling & Simulation Kristian Debus
A single-phase, non-isothermal model for PEM fuel cells Hyunchul Ju, Hua Meng, Chao-Yang Wang 5月 1, 2005
A Study of Jumper FIV Due to Multiphase Internal Flow: Understanding Life-Cycle Fatigue Alan Mueller, PhD
A Study of Reynolds Number Effects on Production Class 8 Tractor-Trailer Combinations Bhaskar Bhatnagar, Dinesh M, Mohan C
A Study of the FIV of a Subsear Jumper due to Multi-phase Internal Flow with an Objective of Understanding Life-cycle Fatigue Alan Mueller
A study of the losses and interaction between one or more bow thrusters and a catamaran hull L Boddy , T Clarke 5月 7, 2013

ページ