Blog

With the release of STAR-ICE in STAR-CCM+ v12.06, Siemens PLM is directly addressing the need for more engine simulation capabilities by offering fast and simple setup of in-cylinder simulations directly within STAR-CCM+. This first release will address the setup of cold flow simulations for multi-valve engines with the automated setup of mesh motion, allowing the user to go from raw CAD geometry to running simulation in just minutes. Default settings and automatically-created post-processing output are aimed at giving the engine engineer a “running start” and mean that you don’t need to be a CFD expert to setup and run one of the most challenging CFD simulations around!

If you haven’t had your head under a rock lately, you’ve seen the headlines. Here, let me get you fully up to speed on the latest:

Diesel recall: which cars are affected, will my MPG decrease, and should I still buy a diesel?

Volkswagen reaches deal for remaining 80,000 Dieselgate vehicles

FCA accused by EPA of failing to disclose software allowing excess diesel emissions

Now I’m not here to postulate the hows and whys any given manufacturer has chosen to use any so-called “defeat devices” or point any fingers of blame, but I will speculate that the diesel engine isn’t doomed or disappearing anytime soon. While I personally prefer the sound and response of an old-fashioned, naturally aspirated gasoline V8, Rudolf Diesel definitely invented the workhorse of the IC engine world back in the late 1800s and it’s hard to not appreciate it for what it is. Its prevalence globally in passenger cars is significant, but it’s even more prolific when you look at how many are used for on-highway medium and heavy-duty trucking applications, off-highway usage, marine, industrial, etc. It’s everywhere!

So we currently face some very difficult challenges to reduce harmful emissions within required limits with governments worldwide constantly tightening those limits. It’s a very difficult problem to address, but it’s not in our nature to just back down from difficult problems, pack up our toys and go home! We engineers want to help solve those difficult problems, don’t we! In the long term, that may mean finding a suitable replacement for the IC engine (there’s plenty of activity in this area right now and, undoubtedly, more coming), but in the short term this means working smarter with better tools to reduce the output of harmful emissions, improve the performance (power) and efficiency (fuel economy), reduce the size/weight and reduce the cost of the diesel engine.

For many years, CD-adapco has been the market leader for Internal Combustion Engine (ICE) simulation.

A key feature in the latest release of DARS, v3.02, is a new laminar flame speed library generator for the ECFM combustion models in STAR-CD/es-ice. This feature improves the accuracy of in-cylinder combustion simulations, allowing for better design of combustion systems to provide more performance with lower fuel consumption and lower emissions.

Subscribe to RSS - Patrick Niven's blog
Matthew Godo
STAR-CCM+ Product Manager
Stephen Ferguson
Marketing Director
James Clement
STAR-CCM+ Product Manager
Joel Davison
Lead Product Manager, STAR-CCM+
Dr Mesh
Meshing Guru
Ravindra Aglave
Director - Chemical Processing
Karin Frojd
Sabine Goodwin
Director, Product Marketing