Blog
Printer-friendly versionPDF version

When it comes to systems, one of the most complex (and perhaps least understood) of all is that of the human body. The average adult human body is, on average, 57% - 60% water. That's a lot of fluid! So it stands to reason that CFD is a great tool for simulating the systems of things like medical implants, surgical techniques, diagnostic systems and the like.

A recent artilce published in Desktop Engineering examines how CFD is making an impact in the medical field. Our own Krisitan Debus Ph.D. talks about our work with an ASME sub-committee, writing verification and validation guidelines for biomedical devices as well as STAR-CCM+'s very useful overset mesh feature. Read the entire article here.

Matthew Godo
STAR-CCM+ Product Manager
Stephen Ferguson
Marketing Director
Brigid Blaschak
Communications Specialist
James Clement
STAR-CCM+ Product Manager
Joel Davison
Lead Product Manager, STAR-CCM+
Dr Mesh
Meshing Guru
Ravindra Aglave
Director - Chemical Processing
Sabine Goodwin
Director, Product Marketing