Blog

We’re conditioned to make comparisons and we do this constantly. Were you able to find any differences between the two images? Or were you perhaps a little frustrated? We have pretty strong reactions when we expect to see differences but can’t find them right away. How about instant replays in (American) football? A receiver makes a catch near the sidelines – quick, was he in or out of bounds? From the first camera angle we’re presented with, there’s no way to tell. We wait impatiently for the updated camera angle replay where “we” can actually make a decision.

Perhaps you have heard it said, such as in the article titled “The Newly Proposed Pump Regulation by the Department of Energy” by Empowering Pumps.

“It has been estimated that 20% of the total energy consumed worldwide is used to run a pump of one sort or another. In addition, of those pumps, two-thirds use 60% more energy than is required.”

So it is no surprise that new standards for pump efficiency have either already been implemented or are being considered by the U.S. Department of Energy (DOE) and the European Union (EU). And given our global focus on energy conservation, it’s reasonable to think that this same type of governmental regulation will be implemented around the world before long.

So, for pump companies, the opportunity and the need are both clear: design more efficient pumps!

Cool is a hard thing to define. It’s completely subjective. But you know it when you see it.

There are a lot of ways to present CAE/CFD data. Plots and tables are arguably what we make most of our decisions on. But, “Excel sheets… aren’t everyone’s friend” . Scenes then… you can put a lot of things into your scenes; results on the surfaces of the thing you’re simulating, streamlines that go in and around the thing you’re simulating… These visual abstractions are a deeply ingrained part of our engineering culture. But not everyone has a casual familiarity with this language. People with diverse levels of expertise have to make sense of these abstractions. And those who don’t, or no longer, speak the language daily and who typically have the least amount of time to assemble conclusions, also carry the heaviest decision-making obligations.

Maybe some of you are getting ahead of me here, recalling the phrase “Color For Directors,” a phrase I personally find to be demeaning to directors and dismissive of what we do. Cool pictures? Sure, but cool isn’t cool if it isn’t right. I submit that we have an ethical obligation to maintain the fidelity of our data , and taking it a step further, we rely on good fundamental data to make decisions. Now, data alone can’t capture an idea . Effective visualizations (cool is implied here) can capture ideas, quickly and easily, inviting curiosity and engaging broader audiences. In STAR-CCM+® v12.02, you can create photorealistic images and animations, reducing the gap between the time needed for you to communicate your messages and the time needed for others to understand practical implications, quickly placing your information into their own knowledge frameworks.

We all have seen electric cars on the street. They look very futuristic and demand a second glance from passers-by. And the convenience… you can drive them in the car pool lane, park and even charge it for free in some places. Great! Their price tag is still an impediment to their large adoption by consumers, though, even if incentives exist in many countries.

Another reason for their slow expansion is the rather low drive range these vehicles offer. The longest range available on the market is 300 km (a little over 186 miles) in real driving conditions. Although this would be sufficient for the usual daily commute from home to office, people have the feeling this is not enough for the few times a year they’ve got to drive 500 km (over 310 miles), like to go celebrate Grandma’s 90th birthday. Well, we don’t call that selfishness - although we think you should visit Grandma more often - we call this range anxiety, or the fear of being short of gas (or electricity in our case). So that’s 300 km you can do before you have got to spend several hours at the charging station to continue on your journey and be on time for Grandma’s cake. You’d better order a three-course meal, with a long coffee, buy some newspapers and hoover the car to occupy your time while the car is charging. Fortunately, there is a solution to reduce your entertainment bill at the service; it is Fast Charging. If we could charge our EV to full capacity in the same time as we fill our gasoline tanks, range anxiety would not be such a problem.

In this blog, we want to explore the complex problem of fast charging with Battery Design StudioTM, understand its implications and see whether there is anything that can be done to remedy this problem.

High temperature processes are of vital importance in a number of industries, including cement, chemical, glass, metallurgy, refining and steel. With so many factors affecting the operational efficiency to consider, the stakes are pretty high for engineers to deliver a safe, reliable, efficient and environmentally friendly operation.

That is why computational fluid dynamics (CFD) and reaction kinetic simulations of combustion processes to design systems are being increasingly utilized. They not only give the necessary insight into the complex physics but also help to significantly lower the cost of iterating between trials and prototypes.

This is important when it comes to improving the current designs of processes and equipment such as gas and coal burners, glass and steel treatment furnaces, process and crude heaters, reformers and dryers and kilns.

My 6-year old son entered my office when I was working on the video below. He looked at it with amazement and asked me “Oh! Mummy, is that real fire?!” I stopped for a second to think and then answered “Kind of. It is real fire, but in the computer. We calculate how the real fire burns.” After a half-impressed and half-puzzled “wow!?” he cheerily jumped out of my office again and probably forgot all about it within 2 minutes.

Charts are important - they play a primary role in decision-making when it comes to evaluating CFD results. Have you ever counted how often you change a chart after you’ve first created it? I’ll speculate it’s more than you think… you’ll probably want to change line and symbol colors and styles, change the range on both axes, change the fonts, and then change the colors again… these picks and clicks and scrolls take time. If you are using Excel or Matlab to create your charts, you lose the implicit connection between the chart and the data sources within your .sim file - going back and forth between the two costs you more time. Worse still, if you’re used to a certain plotting package, there are differences compared to STAR-CCM+® on where in the UI you need to make those changes. In having to switch back and forth between plotting packages, the time spent looking for where you need to make a change is potentially greater than the time needed to actually make it. To understand and communicate the information your charts contain more quickly, and to make your finalized charts faster in STAR-CCM+, version 12.02 introduces Chart Highlighting.

Software development is sometimes similar to raising a child. After the excitement of a new arrival with tentative steps and the promise of great things in the future, it develops into a moody teenager, usually working well but prone to tantrums. The final stage for both children and software is a graduation to a responsible adult, working well, providing benefits, and giving great results.

Has EHP finally taken the last step and matured? Has the prodigy child finally turned into a responsible adult? Ever since its inception and first tentative steps in the market as an add-on, we at Siemens PLM and our clients have had to live with its tantrums and acts of genuine helpfulness. The teenage years were particularly difficult, not wanting to move on from version 9.06 while its big brother STAR-CCM+® went seamlessly through its three releases per year gears.

Matthew Godo
STAR-CCM+ Product Manager
Stephen Ferguson
Marketing Director
James Clement
STAR-CCM+ Product Manager
Joel Davison
Lead Product Manager, STAR-CCM+
Dr Mesh
Meshing Guru
Ravindra Aglave
Director - Chemical Processing
Karin Frojd
Sabine Goodwin
Director, Product Marketing