Blog

The Paris Agreement, adopted by consensus by all of the 195 NFCCC (United Nations Framework Convention on Climate Change) participating countries at the end of COP21 in December 2015, sets an ambitious target to limit global warming to well below 2°C. Although this agreement hasn’t entered into force yet, and will only do so if 55 countries that produce at least 55% of the world's GHG (greenhouse gas) emissions ratify, accept, approve or accede to the agreement when it opens for signature in April 2016, the very fact that such a consensus was reached shows a global willingness and readiness for change.

But change is always uncomfortable. The Paris Agreement will impact industries in numerous sectors and may push them to the limits of their financial, computational, human, and time resources: How will they be able to keep up with the innovation pace? How can we shift mindsets so industries prioritize environmental-friendly solutions over profitable solutions? And to which extent will business models need to change to be viable?
Using Engineering Simulation to Foster Innovation in the Fight Against Climate Change

For both undergraduate and graduate students, fluid mechanics courses can be challenging. In addition to learning theories and complex computations, many courses require a project or two that demonstrates the student's ability to create a simulation model. So how many professors and lecturers teach only theory and what percentage combine theory with an open-source or commercial CFD code?

Our annual STAR Global Conference is a great way of or observing the state of the simulation market, and the extent to which the things that we were talking about as “bleeding edge” at the previous conferences are not only finding leverage, but often becoming “the norm” in industrial usage.

I spent nearly the whole SGC locked up in a dark room interviewing our customers for video testimonials. It was an incredibly motivating and inspiring, and frankly exhausting experience. The twenty or so customers that I interviewed confronted me with so much passion about their simulation processes that at times it felt like being at a religious “revival” meeting than an engineering simulation conference.

Here is what I learned from SGC16.

Workflow automation and ease of use continue to be a focus of STAR-CCM+ v11.02. Reference geometries such as points, planes, axes and coordinate systems can now be created on a component in 3D-CAD. These entities will remain ‘pinned’ to the geometry they are created from, making it easy to build more complex geometries and enabling automated design exploration.

Admixtus, a virtual product development (VPD) tool for performing mixing simulations, will drop the barrier for engineers active in the field looking to solve problems and optimize processes. They can introduce simulation with the help of Admixtus as a modern engineering tool in their toolset of problem solving and keep on expanding its applicability based on the strength of a wide variety of multi-physics capabilities in STAR-CCM+.

Following a super-charged Saturday and a high-tension Super Sunday last weekend, Land Rover BAR won the Louis Vuitton America’s Cup World Series Oman and became the only team to win two ACWS events in the season to date.
Land Rover BAR victorious in Oman

Matthew Godo
STAR-CCM+ Product Manager
Stephen Ferguson
Marketing Director
James Clement
STAR-CCM+ Product Manager
Dr Mesh
Meshing Guru
Joel Davison
Lead Product Manager, STAR-CCM+
Ravindra Aglave
Director - Chemical Processing
Karin Frojd
Sabine Goodwin
Director, Product Marketing